This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-EXP430G2_LaunchPad



MSP-EXP430G2_LaunchPad能直接驱动BTL003段式液晶片吗?

  • 可以但是最好使用共阳极的方式,让MCU 的IO工作在拉电流方式,同时注意限流电阻最好大一点,MCU的电流承载能力很弱,单个IO不能超过6mA,整体不超过40mA(拉电流)

  • 可以但是最好使用共阳极的方式,让MCU 的IO工作在拉电流方式,同时注意限流电阻最好大一点,MCU的电流承载能力很弱,单个IO不能超过6mA,整体不超过40mA(拉电流)

  • 此液晶是4MUX,1//3Bias的,驱动起来比较麻烦,每一个I/O口都要配分压电阻,且配合合适的I/O口寄存器配置。液晶的MUX和Bias的值不同,对I/O口电压时序要求会不同。在TI官网,搜索代码为SLAA516的文档,里面有详细说明,是TI工程师设计的解决方案,但是是针对1/2Bias液晶的。对于//3Bias的液晶,用文档中的扫描时序得到的显示效果不好。

    我做了4MUX,1//3Bias的液晶驱动代码和文档,但现在还没发布。注意此办法功耗较大,适用于对功耗要求不严格,对成本要求严格的场合,一般来说就是交流供电的低成本显示应用。

  • Hi Fiona,

    请问1/3Bias的驱动代码现在发布了吗?是否可以共享一下?谢谢!