This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

咨询MSP430F6736



你好 我想咨询6736这个型号数字以及模拟部分电源输出是什么意思,是个芯片的数字 模拟电源供电还是怎么的,LCDCAP不用是不是直接接GND,VCORE管脚怎么处理,Thanks  qq359566900

  • 1.使用LCD时,LCDCAP接4.7UF电容到DVSS,如果不使用LCD则将LCDCAP直接接到DVSS;

    2.VCORE是CPU内核电压引脚,应该接470NF电容到DVSS,VCORE根型号不同,约有区别,大约在1.8V左右,详细资料见F6736的datasheet,注意VCORE不能接外部负载,仅供内部使用。

    3.MCU数字与模拟的电源是分开的,有DVCC,DVSS,VDSYS(接4.7UF滤波电容)和AVCC,AVSS,VASYS(接4.7UF滤波电容),注意datasheet里面的说明。一般在外部可设计成π型滤波,VSS可接在一起,注意单点接地。