最近在使用MSP430AFE253的SD_24进行数据采集,使用的是外部的1.25V的基准电源,但是3块板子的AD输出的数据都衰减了,只有理论输出的84%。不知道是什么原因,请专家指导一下!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最近在使用MSP430AFE253的SD_24进行数据采集,使用的是外部的1.25V的基准电源,但是3块板子的AD输出的数据都衰减了,只有理论输出的84%。不知道是什么原因,请专家指导一下!
你好,
不确定你是否有通过中断方式获取值? 同时加入一段延时如下:
for (i = 0; i < 0x3600; i++); // Delay for 1.2V ref startup
SD24CCTL2 |= SD24SC; // Set bit to start conversion
__bis_SR_register(LPM0_bits + GIE); // Enter LPM0 w/ interrupts
}
是否有改善?