This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F169 DCO频率设置问题

进行如下设置时,提示CALBC1_8MHZ与CALDCO_8MHZ未定义。是否因为缺少头文件?

BCSCTL1 = CALBC1_8MHZ; // Set range

DCOCTL = CALDCO_8MHZ; // Set DCO step + modulation

  • 你可以打开头文件看看有没有CALBC1_8MHZ与CALDCO_8MHZ的定义。

    我记得f169的信息flash内好像没有这两个校准数据,所以头文件里也没有。

  • 头文件里面的确没有定义,那我如何通过内部的DCO获得准确的8M晶振呢?还是必须外接8M的晶振?

  •  参考范例代码。

    //******************************************************************************
    //  MSP-FET430P140 Demo - Basic Clock, Implement Auto RSEL SW FLL
    //
    //  Description: Set DCO clock to (Delta)*(4096) using software FLL. DCO clock
    //  is output on P5.5 as SMCLK.  DCO clock, which is the selected SMCLK source
    //  for timer_A is integrated over LFXT1/8 (4096) until SMCLK is is equal
    //  to Delta.  CCR2 captures ACLK.  To use Set_DCO Timer_A must be
    //  operating in continous mode.  Watch crystal for ACLK is required for
    //  this example.  Delta must be kept in a range that allows possible
    //  DCO speeds.  Minimum Delta must ensure that Set_DCO loop
    //  can complete within capture interval. Maximum delta can be calculated be
    //  f(DCOx7) / 4096.  f(DCOx7) can be found in device specific datasheet.
    //  ACLK = LFXT1/8 = 32768/8, MCLK = SMCLK = target DCO
    //  //* External watch crystal installed on XIN XOUT is required for ACLK *//	
    //
    //           MSP430F149
    //         ---------------
    //     /|\|            XIN|-
    //      | |               | 32kHz
    //      --|RST        XOUT|-
    //        |               |
    //        |           P5.5|--> SMLCK = target DCO
    //        |           P5.6|--> ALCK = 4096
    //
    //
    //  M. Buccini
    //  Texas Instruments Inc.
    //  Feb 2005
    //  Built with CCE Version: 3.2.0 and IAR Embedded Workbench Version: 3.21A
    //******************************************************************************
    
    #include <msp430.h>
    
    void Set_DCO (void);
    
    int main(void)
    {
      WDTCTL = WDTPW + WDTHOLD;                 // Stop WDT
      P5DIR |= 0x60;                            // P5.5,6 output
      P5SEL |= 0x60;                            // P5.5,6 SMCLK, ACLK output
      Set_DCO();                                // Set DCO
    
      while (1);
    }
    
    //------------------------------------------------------------------------------
    void Set_DCO (void)                         // Set DCO to selected frequency
    //------------------------------------------------------------------------------
    {
    //#define DELTA 900                           // target DCO = DELTA*(4096) = 3686400
    #define DELTA 256                           // target DCO = DELTA*(4096) = 1048576
    //#define DELTA 70                            // target DCO = DELTA*(4096) = 286720
      unsigned int Compare, Oldcapture = 0;
    
      BCSCTL1 |= DIVA_3;                        // ACLK= LFXT1CLK/8
      CCTL2 = CM_1 + CCIS_1 + CAP;              // CAP, ACLK
      TACTL = TASSEL_2 + MC_2 + TACLR;          // SMCLK, cont-mode, clear
    
      while (1)
      {
        while (!(CCIFG & CCTL2));               // Wait until capture occured
        CCTL2 &= ~CCIFG;                        // Capture occured, clear flag
        Compare = CCR2;                         // Get current captured SMCLK
        Compare = Compare - Oldcapture;         // SMCLK difference
        Oldcapture = CCR2;                      // Save current captured SMCLK
    
        if (DELTA == Compare) break;            // If equal, leave "while(1)"
        else if (DELTA < Compare)               // DCO is too fast, slow it down
        {
          DCOCTL--;
          if (DCOCTL == 0xFF)
          {
            if (!(BCSCTL1 == (XT2OFF + DIVA_3)))
            BCSCTL1--;                          // Did DCO roll under?, Sel lower RSEL
          }
        }
        else
        {
          DCOCTL++;
          if (DCOCTL == 0x00)
            {
              if (!(BCSCTL1 == (XT2OFF + DIVA_3 + 0x07)))
              BCSCTL1++;                        // Did DCO roll over? Sel higher RSEL
            }
        }
      }
      CCTL2 = 0;                                // Stop CCR2
      TACTL = 0;                                // Stop Timer_A
    }