Other Parts Discussed in Thread: MSP430G2553, MSP430G2253
这个程序为什么按下按键p1.3无中断响应?这是由产生pwm波的程序和ad采样显示(lcd1602)合成的,在产生pwm波的程序里p1.3可以响应。
#include "msp430g2553.h"
#include "lcd1602.c"
#define uchar unsigned char
#define uint unsigned int
uint a[11]={0},num; //定义数组用于储存采样值
uint shi=0,shifen=0,gewei=0,baifen=0,baifen1=0,shi1=0,shifen1=0,gewei1=0;
long P10=0,P11=0,P10_V=0,P11_V=0,A=0,A1=0; //定义变量
uchar table[]={0x30,0x31,0x32,0x33,0x34,0x35,0x36,0x37,0x38,0x39}; //0~9
void ADC10_init(); //声明ADC10初始化函数
void display(); //显示函数
void pwm();
void main()
{ WDTCTL = WDTPW + WDTHOLD; //关狗
LCD_init_first();
LCD_init();
ADC10_init(); //初始化ADC10
while(1)
{
pwm();
ADC10CTL0 &=~ ENC; //禁用ADC10的Conversion
while(ADC10CTL1 & ADC10BUSY); //测忙
ADC10SA= (unsigned int)a; //获取a[]的首地址
ADC10CTL0 |= ADC10SC + ENC; //启动ADC10
_BIS_SR(LPM0_bits+GIE); //低功耗模式0,开中断
P10=a[1]+a[3]+a[5]+a[7]; //将A0采样值相加
P10= P10/4.0; //求平均值
P10_V = P10*250/1023; //转化为电压并乘以100
display(); //显示
}
}
void display()
{ uint P10_int;
P10_int=(uint)P10_V;
/*求A0采样的各个位*/
A=-14*P10_int+1733.3;
shi = A/1000; //求个位
gewei =(A%1000)/100; //求十分位
shifen =((A%1000)%100)/10; //求百分位
baifen =((A%1000)%100)%10;
/*显示A0处的值*/
LCD_write_command(0x80);
LCD_write_data(table[shi]);
LCD_write_data(table[gewei]);
LCD_write_data('.');
LCD_write_data(table[shifen]);
LCD_write_data(table[baifen]);
LCD_write_data('V');
}
void ADC10_init()
{
/* ADC中断使能+打开ADC10+打开基准生成电压+采样保持时间16*ADC10CLK+(VREF+ and VR-=AVS)+ADC10 multi+2.5V */
ADC10CTL0 = ADC10IE + ADC10ON + REFON + ADC10SHT_2 + SREF_1 + MSC + REF2_5V;
/* 重复序列转换+时钟源选择ADC10OSC+0分频+选择channel1 */
ADC10CTL1 = CONSEQ_3 + + ADC10DIV_0 + INCH_1;
ADC10AE0 |=BIT0+BIT1+BIT3; //打开模拟输入通道
ADC10DTC1 |= 0X08; //采样数为8
}
void pwm()
{
P1SEL |= BIT2;
P1DIR |= BIT2; // P1.2 as TA0.1 output
P1REN |= BIT3;
P1IES |= BIT3; //P1.3 high to low interrupt
_EINT();
P1IFG = 0;
P1IE |= BIT3; //Enable P1.3 interrupt
CCTL1 = OUTMOD_3; /* PWM output mode: 3 - PWM set/reset */
CCR0 = 195;
CCR1 = 15;
TACTL = TASSEL_2 + TACLR + MC_1; // SMCLK, UP mode.
__low_power_mode_0();
}
/*#pragma vector=ADC10_VECTOR
__interrupt void ADC10_ISR(void)
{
__bic_SR_register_on_exit(CPUOFF); //唤醒CPU
}*/
#pragma vector = PORT1_VECTOR
__interrupt void port1_isr(void)
{
if (P1IFG & BIT3)
{
for(int i=0; i<10; i++);
CCR1 += 15;
if (CCR1 > 195)
CCR1 = 0;
P1IFG &= ~BIT3;
}
}
这是lcd1602的程序
#include <intrinsics.h>
#include <msp430g2253.h>
#include <msp430.h>
/*****************************************************
端口定义
****************************************************/
#define LCD_EN_PORT P1OUT //以下2个要设为同一个口
#define LCD_EN_DDR P1DIR
#define LCD_RS_PORT P1OUT //以下2个要设为同一个口
#define LCD_RS_DDR P1DIR
#define LCD_DATA_PORT P2OUT //以下3个要设为同一个口
#define LCD_DATA_DDR P2DIR //一定要用高4位
#define LCD_RS BIT6
#define LCD_EN BIT7
#define LCD_DATA BIT7|BIT6|BIT5|BIT4 //4位数据线连接模式
/***************************************************
预定义函数
**************************************************/
void LCD_init(void);
void LCD_init_first(void);
void LCD_en_write1(void); //上升沿使能
void LCD_en_write2(void); //下降沿使能
void LCD_write_command(unsigned char command);
void LCD_write_data(unsigned char data);
void LCD_set_xy (unsigned char x, unsigned char y);
void LCD_write_string(unsigned char X,unsigned char Y, unsigned char *s);
void LCD_write_char(unsigned char X,unsigned char Y, unsigned char data);
void delay_1ms(void);
void delay_nus(unsigned int n);
void delay_nms(unsigned int n);
/********************************************
LCD液晶操作函数
*******************************************/
void LCD_init_first(void) //LCD1602液晶初始化函数(热启动)
{
delay_nms(500);
LCD_DATA_DDR|=LCD_DATA; //数据口方向为输出
LCD_EN_DDR|=LCD_EN; //设置EN方向为输出
LCD_RS_DDR|=LCD_RS; //设置RS方向为输出
delay_nms(50);
LCD_write_command(0x30);
delay_nms(50);
LCD_write_command(0x30);
delay_nms(5);
LCD_write_command(0x30);
delay_nms(500);
}
/*****************************************
*
* LCD1602液晶初始化函数
*
****************************************/
void LCD_init(void)
{
delay_nms(500);
LCD_DATA_DDR|=LCD_DATA; //数据口方向为输出
LCD_EN_DDR|=LCD_EN; //设置EN方向为输出
LCD_RS_DDR|=LCD_RS; //设置RS方向为输出
delay_nms(500);
LCD_write_command(0x28); //4位数据接口
delay_nms(50);
LCD_write_command(0x28); //4位数据接口
delay_nms(50);
LCD_write_command(0x28); //4位数据接口
delay_nms(50);
LCD_en_write2();
delay_nms(50);
LCD_write_command(0x28); //4位数据接口
delay_nms(500);
LCD_write_command(0x01); //清屏
LCD_write_command(0x0c); //显示开,关光标,不闪烁
LCD_write_command(0x06); //设定输入方式,增量不移位
delay_nms(50);
}
/*****************************************
*
* 液晶使能上升沿
*
****************************************/
void LCD_en_write1(void)
{
LCD_EN_PORT&=~LCD_EN;
delay_nus(10);
LCD_EN_PORT|=LCD_EN;
}
/*****************************************
*
* 液晶使能下降沿
*
****************************************/
void LCD_en_write2(void)
{
LCD_EN_PORT|=LCD_EN;
delay_nus(10);
LCD_EN_PORT&=~LCD_EN;
}
/*****************************************
*
* 写指令函数
*
****************************************/
void LCD_write_command(unsigned char command)
{
delay_nus(16);
P2SEL=0x00;
LCD_RS_PORT&=~LCD_RS; //RS=0
LCD_en_write1();
LCD_DATA_PORT&=0X0f; //清高四位
LCD_DATA_PORT|=command&0xf0; //写高四位
delay_nus(16);
LCD_en_write2();
command=command<<4; //低四位移到高四位
LCD_en_write1();
LCD_DATA_PORT&=0x0f; //清高四位
LCD_DATA_PORT|=command&0xf0; //写低四位
LCD_en_write2();
}
/*****************************************
*
* 写数据函数
*
****************************************/
void LCD_write_data(unsigned char data)
{
delay_nus(16);
P2SEL=0x00;
LCD_RS_PORT|=LCD_RS; //RS=1
LCD_en_write1(); //E上升沿
LCD_DATA_PORT&=0X0f; //清高四位
LCD_DATA_PORT|=data&0xf0; //写高四位
delay_nus(16);
LCD_en_write2();
data=data<<4; //低四位移到高四位
LCD_en_write1();
LCD_DATA_PORT&=0X0f; //清高四位
LCD_DATA_PORT|=data&0xf0; //写低四位
LCD_en_write2();
}
/*****************************************
*
* 写地址函数
*
****************************************/
void LCD_set_xy( unsigned char x, unsigned char y )
{
unsigned char address;
if (y == 0) address = 0x80 + x;
else address = 0xc0 + x;
LCD_write_command( address);
}
/*****************************************
*
*LCD在任意位置写字符串,列x=0~15,行y=0,1
*
****************************************/
void LCD_write_string(unsigned char X,unsigned char Y,unsigned char *s)
{
LCD_set_xy( X, Y ); //写地址
while (*s) //写显示字符
{
LCD_write_data( *s );
s++;
}
}
/*****************************************
*
* LCD在任意位置写字符,列x=0~15,行y=0,1
*
****************************************/
void LCD_write_char(unsigned char X,unsigned char Y,unsigned char data)
{
LCD_set_xy( X, Y ); //写地址
LCD_write_data( data);
}
/*****************************************
*
* 1us延时函数
*
****************************************/
void delay_1us(void)
{
asm("nop");
}
/*****************************************
*
* N us延时函数
*
****************************************/
void delay_nus(unsigned int n)
{
unsigned int i;
for (i=0;i<n;i++)
delay_1us();
}
/*****************************************
*
* 1ms延时函数
*
****************************************/
void delay_1ms(void)
{
unsigned int i;
for (i=0;i<1140;i++);
}
/*****************************************
*
* N ms延时函数
*
****************************************/
void delay_nms(unsigned int n)
{
unsigned int i=0;
for (i=0;i<n;i++)
delay_1ms();
}