This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

进入低功耗模式,电流下不来

Other Parts Discussed in Thread: MSP430F5438A

用的MSP430F5438A,最小系统,没有外面电路,直接用3V的稳压电源供电的,

程序设置进入低功耗模式LMP3,但是电流一直在3mA,和没有进低功耗模式一样的。IO口配置成输入或者出入都是电流在3mA左右。

晶振使用的内部或者外面的32.768KHZ都一样的

测试如下:

#include <msp430F5438A.h>

#define uchar unsigned char
#define uint unsigned int
#define ulong unsigned long int

#define CPU_F ((double)1045000UL) //XT2 --> 24MHZ
#define Delay_us(x) __delay_cycles((long)(CPU_F*(double)x/1000000.0)) //延时1us
#define Delay_ms(x) __delay_cycles((long)(CPU_F*(double)x/1000.0)) //延时1ms

#define INPUT 0
#define OUTPUT 1

#define HIGH 1
#define LOW 0

#define PORT_DIR INPUT
#define OUT_LEVEL LOW


void Set_Vcore(uint level);
void SysClock_Init();
void GPIO_Init();
void SVSM_Off(void);

/******************************************************************************/
char i=0;

void main(void) //主函数
{
/* 1. 关闭看门狗 */
WDTCTL = WDTPW + WDTHOLD;

/* 2. 初始化系统时钟和设置内核电压 */
// Set_Vcore(PMMCOREV_1);
SysClock_Init();

/* 3. 初始化外设状态 */
GPIO_Init();


// /* 4. 开中断 */
__bis_SR_register(GIE);

/* 5. 执行循环 */
while(1)
{
i++;
SVSM_Off();  //关闭SVS ,SVM
__bis_SR_register(LPM4_bits);
__no_operation();

i++;
if ( i > 10 )
i = 0;
}
}
/************************************END***************************************/

/******************************************************************************
函数: void SysClock_Init()
功能: 初始化时钟,使用内部晶振32768HZ作为:ACLK、MCLK、SMLK
参数: 无
返回值:无
说明:
******************************************************************************/
void SysClock_Init()
{

       UCSCTL4 |= SELA__XT1CLK + SELM__XT1CLK + SELS__XT1CLK; //选择ACLK、MCLK、SMCLK为REFOCLK

}

/******************************************************************************
函数: void GPIO_Init()
功能: 端口初始化
参数:
返回值:
说明:
******************************************************************************/
void GPIO_Init()
{
//P1
P1SEL = 0;
P1DIR = PORT_DIR;
P1OUT = OUT_LEVEL;

P2SEL = 0;
P2DIR = PORT_DIR;
P2OUT = OUT_LEVEL;

P3SEL = 0;
P3DIR = PORT_DIR;
P3OUT = OUT_LEVEL;

P4SEL = 0;
P4DIR = PORT_DIR;
P4OUT = OUT_LEVEL;

P5SEL = 0;
P5DIR = PORT_DIR;
P5OUT = OUT_LEVEL;

P6SEL = 0;
P6DIR = PORT_DIR;
P6OUT = OUT_LEVEL;

P7SEL |= BIT0 + BIT1;
// P7DIR = PORT_DIR;
// P7OUT = OUT_LEVEL;

P8SEL = 0;
P8DIR = PORT_DIR;
P8OUT = OUT_LEVEL;

P9SEL = 0;
P9DIR = PORT_DIR;
P9OUT = OUT_LEVEL;

P10SEL = 0;
P10DIR = PORT_DIR;
P10OUT = OUT_LEVEL;

P11SEL = 0;
P11DIR = PORT_DIR;
P11OUT = OUT_LEVEL;

PJDIR = PORT_DIR;
PJOUT = OUT_LEVEL;

// P1DIR |= BIT3 + BIT4 + BIT5 + BIT6; //LED IO设置为输出
// P1OUT &= ~(BIT3 + BIT4 + BIT5 + BIT6); //LED灭
}

/******************************************************************************
函数: void Set_Vcore(uint level)
功能: 设置内核电压
参数: Power Management M
返回值:
说明:
******************************************************************************/
void Set_Vcore(uint level)
{
PMMCTL0_H = PMMPW_H; // Open PMM registers for write

SVSMHCTL = SVSHE + SVSHRVL0 * level + SVMHE + SVSMHRRL0 * level; // Set SVS/SVM high side new level

SVSMLCTL = SVSLE + SVMLE + SVSMLRRL0 * level; // Set SVM low side to new level
while ((PMMIFG & SVSMLDLYIFG) == 0); // Wait till SVM is settled

PMMIFG &= ~(SVMLVLRIFG + SVMLIFG); // Clear already set flags

PMMCTL0_L = PMMCOREV0 * level; // Set VCore to new level
if ((PMMIFG & SVMLIFG)) // Wait till new level reached
while ((PMMIFG & SVMLVLRIFG) == 0);

SVSMLCTL = SVSLE + SVSLRVL0 * level + SVMLE + SVSMLRRL0 * level; // Set SVS/SVM low side to new level

PMMCTL0_H = 0x00; // Lock PMM registers for write access
}

void SVSM_Off(void)
{
PMMCTL0_H = PMMPW_H;
SVSMHCTL &= ~(SVMHE + SVSHE);
SVSMLCTL &= ~(SVSLE + SVMLE);
PMMCTL0_H = 0x00;
}