This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Sat Aug 13, 2016 16:39:29: Failed to load flash loader: C:\work\msp430\G2553\PWM\PWM_2.dep

Other Parts Discussed in Thread: MSP430G2553

 用fet430uif不能下载程序 老报错 请问什么问题  iar5.3

  • 根据楼主提供的信息,可能的原因比较多:

    1、不知道楼主用的什么烧写软件,有可能烧写软件不支持这个ic。建议使用最新的ccs或者iar试试

    2、接插件或相关线路接触不良,建议检察接插件连接情况,以及pcb走线是否连接良好

    3、软件设置问题,检查上位机设置的usb口是否是fet430uif

    4、电路问题,检查RST引脚和GND间电容,一般要求不大于10uF。

  • 用iar5.3烧写 上面能选g2553 线路都接好了  用2线下载方式时候  能仿真 运行  能download active application

    接插件都接触良好   rst 与gnd之间 加了0.1uf电容电容正到3.3v加10k电阻。   usb设置的是fet430uif

  • 请问 有 MSP430G2553的标准原理图么  能否传一份!