This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UART 无法接收

Other Parts Discussed in Thread: MSP430G2553

IAR 5.4

#include "msp430g2553.h"
typedef unsigned char uint8;
typedef unsigned int  uint16 ;


volatile unsigned char RxByte;

void CLK_Init();

void UART_Init(void);
void UART_Tx1Byte(unsigned char Txdata);
void UART_TxString(unsigned char *pTxString);

unsigned char su[]="hello world!!!";

void main(void)
{

  WDTCTL = WDTPW + WDTHOLD;                 // Stop watchdog timer

  CLK_Init();
  UART_Init();

  UART_TxString(su);
  _NOP();

  __bis_SR_register(LPM3 + GIE);       // Enter LPM3 w/ interrupts enabled
}


#pragma vector = USCIAB0RX_VECTOR
__interrupt void USCI0RX_ISR(void)
{
    P1DIR |= BIT6;
    P1OUT |= BIT6;
    RxByte = UCA0RXBUF;                        // Display RX'ed charater
}


void CLK_Init()
{
    if (CALBC1_1MHZ ==0xFF || CALDCO_1MHZ == 0xFF)
    {
        while(1);               // 挂起
    }
    BCSCTL1  = CALBC1_1MHZ;
    DCOCTL   = CALDCO_1MHZ;     //设置DCO模式
    BCSCTL3 |= LFXT1S_0;
    while(IFG1 & OFIFG)
    {
        IFG1 &= ~OFIFG;         //清除OSCFault 标志
        __delay_cycles(100000); //为可见标志延时
    }
}



void UART_Init(void)
{
    /*外部功能选择*/
    P1SEL  = BIT1 + BIT2 ;          // P1.1 = RXD, P1.2=TXD
    P1SEL2 = BIT1 + BIT2;
    /*选择时钟*/
    UCA0CTL1 |= UCSSEL_1;           // CLK = SMCLK
    /*选择波特率*/
    UCA0BR0 = 0x03;                 // 32kHz/9600 = 3.41
    UCA0BR1 = 0x00;
    UCA0MCTL = UCBRS1 + UCBRS0;     // Modulation UCBRSx = 3
    /**/
    UCA0CTL1 &= ~UCSWRST;           // **Initialize USCI state machine**
    IE2 |= UCA0RXIE ;               // Enable USCI_A0 RX interrupt
}

void UART_Tx1Byte(unsigned char TxByte)
{
  while(UCA0STAT & UCBUSY);
  UCA0TXBUF = TxByte;
}

void UART_TxString(unsigned char *pTxString)
{
    while(*pTxString)
    {
        UART_Tx1Byte(*pTxString++);
    }
}

 

通过串口调试助手发送毫无压力但是不能接收 ,调试发现死活 进入不了接收中断啊 ,

而且试了一下官方的例子(已改为HW) , 也不能进入啊

怎么回事啊

该怎么做 , 详细一点

  • 1.程序里面配置的USCI-A模块即UART的时钟是SMCLK,但是主程序最后一句进入了LPM3模式,这个模式SMCLK是关闭的,所以没办法触发接受中断

    2.需要把USCI-A模块的时钟配置成ACLK或者让MCU只进入LPM0。