Other Parts Discussed in Thread: MSP430F5529
反三角函数,每运行一次差不多3ms,三个反三角函数就要接近10ms
四轴飞控的姿态控制程序,要求200Hz控制一次,每次控制程序运行时间必须在5ms内,其他处理不超过1ms,但是加上3个反三角函数,就要10ms了,没法实现200hz控制频率,有没有什么办法减少这三个反三角函数运算时间,最好每个运行时间不超过1ms。
1、程序放在ram中运行会有效果吗,能不能把用到的math库的反三角函数,放到ram中运行?
2、有什么简便的算法可以实现反三角函数,减低运算时间?
3、MSP430F5529试过超频到42MHz,这样有没有问题?