msp430g2553与msp430g2452单片机资源的区别,速求
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
|
Frequency (MHz) |
16 |
16 |
|
Flash (KB) |
16 |
8 |
|
SRAM (B) |
512 |
256 |
|
GPIO |
24 |
16 |
|
Cap touch I/O |
Yes |
Yes |
|
Timers - 16-bit |
2 |
1 |
|
Watchdog |
Yes |
Yes |
|
Brown Out Reset |
Yes |
Yes |
|
USCI_A (UART/LIN/IrDA/SPI) |
1 |
USI (I2C/SPI)
|
|
USCI_B (I2C & SPI) |
1 |
|
|
Comparators |
Yes |
Yes |
|
Temp Sensor |
Yes |
Yes |
|
ADC |
10-bit SAR |
10-bit SAR |
|
ADC Channels |
8 |
8 |
|
Pin/Package |
0DIESALE, 0WAFERSALE, 20PDIP, 20TSSOP, 28TSSOP, 32QFN |
14TSSOP, 16QFN, 20PDIP, 20TSSOP |
其实可以直接从www.ti.com (MSP430新手入门)上直接找到。或者从附件总表中查看。上面有全系列的MSP430的资源概述。