This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LCD_A使用问题



430的4系列MCU  LCD_A控制器使用内部电阻和外部电阻在功耗和效果有什么区别,俩者具体怎么用,怎么用功耗最低。

  • When using an external resistor divider R33 may serve as a switched-VLCD

    output when VLCDEXT = 0. This allows the power to the resistor ladder to be

    turned off eliminating current consumption when the LCD is not used. When

    VLCDEXT = 1, R33 serves as a VLCD input.

    可以在使用手册里看到,使用外部电阻更能够减小功耗。

  • 1.如果应用中对面积,成本等要求得多,对亮度,功耗要求不是很高,用内部电阻就合适;

    2.如果要节省功耗,亮度调节更细致,则使用外部电阻,但是会增加PCB的面积和成本