This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5529 IIC接口 OLED12864驱动程序

OLED12864驱动程序

    暑假电子设计大赛的时候移植到430上的OLED驱动程序,分享给大家。

/********************************************************************
* OLED屏测试程序
* msp430g2553
*
* 调用方法:
*		LCD_Init();  //	OLED 初始化
*		LCD_Fill(0x00);  // 全屏填充 0x00
*		LCD_GBK16(0, 2, "1.锄禾日当午,\r2.汗滴禾下土。\r3.谁知盘中餐,");
*		LCD_P6x8Str (0,4,"OLED"); // 显示6*8  字符串
*		= HowMuchWidth(Num);// 获取某数有几位
*		LCD_IntNum(x, y, HowMuchWidth(v), v); // 显示数字
*		LCD_16Pic(unsigned char x,unsigned char y,unsigned char width,unsigned char dat[]);//16像素高度图片
*		LCD_8Pic(unsigned char x,unsigned char y,unsigned char width,unsigned char ch[]);//8像素高度图片
*		LCD_AllPic(unsigned char dat[]);//全局图像显示
*
*
* 说明:图像取模:纵向取模,字节倒序
*
* 作者:星希望(已校验)
* 日期:2016年7月25日
**********************************************************************/
#include "OLED.h"
#include "OLED_Font.h"
#include "msp430g2553.h"

#define LCD_SCL_1	P2OUT |=  BIT0
#define LCD_SCL_0	P2OUT &= ~BIT0

#define LCD_SDA_1	P2OUT |=  BIT1
#define LCD_SDA_0	P2OUT &= ~BIT1

#define LCD_RST_1	P2OUT |=  BIT2
#define LCD_RST_0	P2OUT &= ~BIT2

#define LCD_DC_1	P2OUT |=  BIT3
#define LCD_DC_0	P2OUT &= ~BIT3


#define XLevelL		0x00
#define XLevelH		0x10
#define XLevel		((XLevelH&0x0F)*16+XLevelL)
#define Max_Column	128
#define Max_Row		64
#define	Brightness	0xCF 

#define X_WIDTH 128
#define Y_WIDTH 64

unsigned int hz16_num = 0; // 汉字个数
//======================================


void LCD_WrDat(unsigned char dat)
{
	unsigned char i=8;
	LCD_DC_1;
	LCD_SCL_0;
	while(i--)
	{
		if(dat&0x80)	{LCD_SDA_1;}
		else			{LCD_SDA_0;}
		LCD_SCL_1; 
		dat<<=1;
		LCD_SCL_0;    
	}
}
void LCD_WrCmd(unsigned char cmd)
{
	unsigned char i=8;
	
	LCD_DC_0;
	LCD_SCL_0;
	while(i--)
	{
		if(cmd&0x80)	{LCD_SDA_1;}
		else			{LCD_SDA_0;}
		LCD_SCL_1;    
		cmd<<=1;
		LCD_SCL_0;   
	} 	
}
void LCD_Set_Pos(unsigned char x, unsigned char y)
{ 
	LCD_WrCmd(0xb0+y);
	LCD_WrCmd(((x&0xf0)>>4)|0x10);
	LCD_WrCmd((x&0x0f)|0x00); 
} 
void LCD_Fill(unsigned char bmp_dat)
{
	unsigned char y, x;
	
	for(y=0;y<8;y++)
	{
		LCD_WrCmd(0xb0+y);
		LCD_WrCmd(0x01);
		LCD_WrCmd(0x10);
		for(x=0;x<X_WIDTH;x++)
			LCD_WrDat(bmp_dat);
	}
}

void LCD_DLY_ms(unsigned int ms)
{                         
	while(ms--)
	{
		__delay_cycles(100);
	}
	return;
}

/*********************************************************************************
* OLED 初始化
*********************************************************************************/
void LCD_Init(void)        
{  
	P2DIR |= BIT0 | BIT1 | BIT2 | BIT3;
  
  	LCD_SCL_1;
	//LCD_CS=1;	//预制SLK和SS为高电平
	LCD_RST_0;
	LCD_DLY_ms(50);
	LCD_RST_1;
	
	/* 计算汉字库的大小 */
	hz16_num = sizeof hz16 / sizeof (struct typFNT_GB162);

	//从上电到下面开始初始化要有足够的时间,即等待RC复位完毕   
	LCD_WrCmd(0xae);//--关闭OLED面板
	LCD_WrCmd(0x00);//---set low column address置低列地址
	LCD_WrCmd(0x10);//---set high column address设置高列地址
	LCD_WrCmd(0x40);//--set start line address  Set Mapping RAM Display Start Line (0x00~0x3F)设置起始行地址设置映射RAM显示起始行(0×00?0x3F之间)
	LCD_WrCmd(0x81);//--set contrast control register设置对比度控制寄存器
	LCD_WrCmd(0xcf);// Set SEG Output Current Brightness设置SEG输出电流亮度
	LCD_WrCmd(0xa1);//--Set SEG/Column Mapping     0xa0左右反置 0xa1正常 设置SEG/列映射0XA0左右反置0xa1正常
	LCD_WrCmd(0xc8);//Set COM/Row Scan Direction   0xc0上下反置 0xc8正常 设置COM/行扫描方向为0xC0上下反置0xc8正常
	LCD_WrCmd(0xa6);//--set normal display	设置正常显示
	LCD_WrCmd(0xa8);//--set multiplex ratio(1 to 64) 设置复用率(1~64)
	LCD_WrCmd(0x3f);//--1/64 duty	 1/64责任
	LCD_WrCmd(0xd3);//-set display offset Shift Mapping RAM Counter (0x00~0x3F)	 置显示失调漂移映射RAM计数器(为0x00?0x3F之间)
	LCD_WrCmd(0x00);//-not offset	 不能抵消
	LCD_WrCmd(0xd5);//--set display clock divide ratio/oscillator frequency	设置显示时钟分频比/振荡器频率
	LCD_WrCmd(0x80);//--set divide ratio, Set Clock as 100 Frames/Sec		设置的分频比,设置时钟为100帧/秒
	LCD_WrCmd(0xd9);//--set pre-charge period	  组预充电期间
	LCD_WrCmd(0xf1);//Set Pre-Charge as 15 Clocks & Discharge as 1 Clock	 设置预充电为15时钟和放电为1时钟
	LCD_WrCmd(0xda);//--set com pins hardware configuration				   组COM插针的硬件配置
	LCD_WrCmd(0x12);
	LCD_WrCmd(0xdb);//--set vcomh
	LCD_WrCmd(0x40);//Set VCOM Deselect Level	 设置VCOM取消等级
	LCD_WrCmd(0x20);//-Set Page Addressing Mode (0x00/0x01/0x02)   设置页面寻址模式(0×00/0×01/0X02)
	LCD_WrCmd(0x02);//
	LCD_WrCmd(0x8d);//--set Charge Pump enable/disable		设置电荷泵启用/禁用
	LCD_WrCmd(0x14);//--set(0x10) disable					设置(0x10)后关闭
	LCD_WrCmd(0xa4);// Disable Entire Display On (0xa4/0xa5)   禁用整个显示屏(0xa4/到0x55)
	LCD_WrCmd(0xa6);// Disable Inverse Display On (0xa6/a7)    禁用逆显示(0xa6/ A7)
	LCD_WrCmd(0xaf);//--turn on oled panel
	LCD_Fill(0x00);  //初始清屏
	LCD_Set_Pos(0,0); 
} 

/*********************************************************************************
* 函数名:LCD_P6x8Str(unsigned char x,unsigned char y,unsigned char *p)
* 功能描述:写入一组标准ASCII字符串
* 参数:显示的位置(x,y),y为页范围0~7,要显示的字符串
* 返回:无
*********************************************************************************/
void LCD_P6x8Str(unsigned char x, unsigned char y, unsigned char ch[])
{
	unsigned char c=0,i=0,j=0;      
	while (ch[j]!='\0')
	{    
		c =ch[j]-32;
		if(x>126 || c==13)	// 下一行
		{x=0;y++;}

		LCD_Set_Pos(x,y);    
		for(i=0;i<6;i++)     
		  LCD_WrDat(F6x8[c][i]);  
		x+=6;
		j++;
	}
}

/*********************************************************************************
* 函数名:LCD_8Pic(unsigned char x,unsigned char y,unsigned char *p)
* 功能描述:写入一组高度为8像素的图标
* 参数:显示的位置(x,y),y为页范围0~7,
* 返回:无
*********************************************************************************/
void LCD_8Pic(unsigned char x,unsigned char y,unsigned char width,unsigned char ch[])
{
	unsigned char j=0;
	
	LCD_Set_Pos(x,y);      
	while (width)
	{         
		LCD_WrDat(ch[j]);  
		j++;
		width--;
	}
}

/*************************************************************************************
* 显示汉字 及 8x16 ascii码
* 坐标x,坐标y,内容
* 查找 hz16[] 结构体数组
*************************************************************************************/
void LCD_GBK16(unsigned int x, unsigned int y, unsigned char *s)
{
	unsigned char j;
	unsigned short k,x0;
	x0=x;

	while(*s) 
	{	
		if((*s) < 128) // ASC段
		{
			k = *s;
			if (k==13) //回车
			{
				x = x0;
				y += 2;
			}
			else 
			{
				if (k>32)	k-=32; //从有效字符开始编码,避开前面的非字符区
				else		k=0;

				LCD_Set_Pos(x, y);
				for(j=0; j<8; j++) 
				{
					LCD_WrDat(F8X16[k*16+j]);	
				}
				LCD_Set_Pos(x, y+1);
				for(j=0; j<8; j++) 
				{
					LCD_WrDat(F8X16[k*16+j+8]);
				}
				x += 8;
			}
			s++;
		}
		else 	// 汉字段
		{
			for(k=0; k<hz16_num; k++) 
			{
				if( (hz16[k].Index[0]==*(s)) && (hz16[k].Index[1]==*(s+1)) )
				{ 
					LCD_Set_Pos(x, y);
					for(j=0; j<16; j++)	//高8位 
					{
						LCD_WrDat(hz16[k].Msk[j]);
					}
					LCD_Set_Pos(x, y+1);
					for(j=0; j<16; j++)	//低8位
					{
						LCD_WrDat(hz16[k].Msk[j+16]);
					}
					break;
				}
			}
			if( k==hz16_num )// 没有找到该汉字
			{
				LCD_Set_Pos(x, y);
				for(j=0; j<16; j++)	//高8位 
				{
					LCD_WrDat(UnknowFont[j]);
				}
				LCD_Set_Pos(x, y+1);
				for(j=0; j<16; j++)	//低8位
				{
					LCD_WrDat(UnknowFont[j+16]);
				}	
			}
			s += 2;
			x += 16;
		}
		if(x>120) {x=0; y+=2;} 
	}	
}

/*********************************************************************************
* 函数名:LCD_16Pic(unsigned char x,unsigned char y,unsigned char *p)
* 参数:x,y		 显示的位置,y为页范围0~7,
* 		width    图标宽度
* 		dat[]    图像数据
*********************************************************************************/
void LCD_16Pic(unsigned char x,unsigned char y,unsigned char width,unsigned char dat[])
{
	unsigned char i=0;
  	LCD_Set_Pos(x, y);
  	for(i = 0;i < width;i++)               
  	{
  		LCD_WrDat(dat[i]);	
  	}      
  	LCD_Set_Pos(x, y + 1); 
  	for(i = 0;i < width;i++)          
  	{
  		LCD_WrDat(dat[i+width]);
  	} 	  	
}
/*********************************************************************************
* 全屏图像显示
*********************************************************************************/
void LCD_AllPic(unsigned char dat[])
{
	unsigned char y, x;
	for(y=0; y<8; y++)
	{	
		LCD_Set_Pos(0, y);
		for(x=0; x<128; x++)
		{
		 	LCD_WrDat(dat[y*128+x]);	
		}
	}
}

/************************************************************************************
* 计算某数有几位
************************************************************************************/
unsigned char HowMuchWidth(unsigned long Num)
{
	unsigned char cnt=0;
	while(Num)
	{
		Num /= 10;
		cnt++;
	}
	return cnt;
}
/************************************************************************************
* 显示数字
* 参数:x,y - 坐标
*		Width- 宽度(有几位数)
*		v	 - 数字
* 说明:右对齐
*************************************************************************************/
void LCD_IntNum(unsigned char x, unsigned char y, unsigned char Width, unsigned long v)
{
	unsigned char a[11];
	unsigned char *p;
	
	// 数位分解
	a[10]= 0;
	a[9] = v    % 10 + '0';
	a[8] = v /10 % 10 + '0';
	a[7] = v /100 % 10 + '0';
	a[6] = v /1000 % 10 + '0';
	a[5] = v /10000 % 10 + '0';
	a[4] = v /100000 % 10 + '0';
	a[3] = v /1000000 % 10 + '0';
	a[2] = v /10000000 % 10 + '0';
	a[1] = v /100000000 % 10 + '0';
	a[0] = v /1000000000 % 10 + '0';
	
	p = &a[10-Width];

	// 显示
	LCD_GBK16(x, y, p); // 显示 8*16  字符串
}

/************************************************************************************
* 显示数字
* 参数:x,y - 坐标
*		Width- 宽度(有几位数)
*		v	 - 数字
* 说明:右对齐
*************************************************************************************/
void LCD_IntNum6x8(unsigned char x, unsigned char y, unsigned char Width, unsigned long v)
{
	unsigned char a[11];
	unsigned char *p;
	
	// 数位分解
	a[10]= 0;
	a[9] = v    % 10 + '0';
	a[8] = v /10 % 10 + '0';
	a[7] = v /100 % 10 + '0';
	a[6] = v /1000 % 10 + '0';
	a[5] = v /10000 % 10 + '0';
	a[4] = v /100000 % 10 + '0';
	a[3] = v /1000000 % 10 + '0';
	a[2] = v /10000000 % 10 + '0';
	a[1] = v /100000000 % 10 + '0';
	a[0] = v /1000000000 % 10 + '0';
	
	p = &a[10-Width];

	// 显示
	LCD_P6x8Str(x, y, p); // 显示 8*16  字符串
}
#ifndef _OLED_H
#define _OLED_H
 
extern unsigned int hz16_num; // 汉字个数

void LCD_Init(void);
void LCD_CLS(void);

void LCD_P6x8Str(unsigned char x,unsigned char y,unsigned char ch[]);
void LCD_GBK16(unsigned int x, unsigned int y, unsigned char *s);

unsigned char HowMuchWidth(unsigned long Num);
void LCD_IntNum(unsigned char x, unsigned char y, unsigned char Width, unsigned long v);
void LCD_IntNum6x8(unsigned char x, unsigned char y, unsigned char Width, unsigned long v);

void LCD_8Pic (unsigned char x,unsigned char y,unsigned char width,unsigned char ch[]);
void LCD_16Pic(unsigned char x,unsigned char y,unsigned char width,unsigned char dat[]);
void LCD_AllPic(unsigned char dat[]);
void LCD_Fill(unsigned char dat);

#endif