This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5438A低功耗问题



int main( void )
{
WDTCTL = WDTPW + WDTHOLD ;
P7SEL |= 0x03 ; // 使能XT1
UCSCTL6 &=~XT1OFF ;
UCSCTL6 |= XCAP_3 ;
UCSCTL4 |= SELA_0 ; // ACLK时钟源选择XT1
UCSCTL5 |= DIVA1 ; // ACLK = XT1/4
P1DIR = 0xFF ; // All P1.x outputs
P1OUT = 0x00 ; // All P1.x reset
P2DIR = 0xFF ; // All P2.x outputs
P2OUT = 0x00 ; // All P2.x reset
P3DIR = 0xFF ; // All P3.x outputs
P3OUT = 0x00 ; // All P3.x reset
P4DIR = 0xFF ; // All P4.x outputs
P4OUT = 0x00 ; // All P4.x reset
P5DIR = 0xFF ; // All P5.x outputs
P5OUT = 0x00 ; // All P5.x reset
P6DIR = 0xFF ; // All P6.x outputs
P6OUT = 0x00 ; // All P6.x reset
P7DIR = 0xFF ; // All P6.x outputs
P7OUT = 0x00 ; // All P6.x reset
P8DIR = 0xFF ; // All P6.x outputs
P8OUT = 0x00 ; // All P6.x reset
P9DIR = 0xFF ; // All P6.x outputs
P9OUT = 0x00 ; // All P6.x reset
P10DIR = 0xFF ; // All P6.x outputs
P10OUT = 0x00 ; // All P6.x reset
P11DIR = 0xFF ; // All P6.x outputs
P11OUT = 0x00 ; // All P6.x reset
SFRIE1 |= WDTIE ; // 使能WDT中断
WDTCTL = WDT_ADLY_1000 ; // 设置WDT为INTERVAL模式,中断间隔1000ms
_EINT() ;

LPM3 ;
for(;;)
{
LPM3 ;
_NOP() ;

__delay_cycles(100) ;

}

如上所图,cpu功耗是445ua,比标称的功耗高很多,不知道怎么回事?时钟对功耗有影响么,我的时钟要设置成8M--,串口波特率较高