This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

如何在MSP430G2553建立组语查表功能 Look Up Table



我使用CCS V6.2 编译一个Sinewave 波形,在TI 组语手册中未查阅到查表(Look Up Table)相关指令及Data 安排正确表示法,(Look Up Table 数据区)

 

我将程序附录于下,请帮我指证错误地方及正确语法, 谢谢您的协助,

Thanks your help. 

;-------------------------------------------------------------------------------
; MSP430 Assembler Code Template for use with TI Code Composer Studio
;
;
;-------------------------------------------------------------------------------
.cdecls C,LIST,"msp430.h" ; Include device header file

;-------------------------------------------------------------------------------
.def RESET ; Export program entry-point to
; make it known to linker.
;-------------------------------------------------------------------------------
.text ; Assemble into program memory.
.retain ; Override ELF conditional linking
; and retain current section.
.retainrefs ; And retain any sections that have
; references to current section.
;-------------------------------------------------------------------------------
; Main loop here
;-------------------------------------------------------------------------------

             RESET                    mov.w #0280h,SP                                         ; Initialize stackpointer
                                              mov.w #WDTPW+WDTHOLD,&WDTCTL ; Stop WDT
                                              bis.b #066h,&P1DIR                                    ; P1.2 and P1.3 output
                                             bis.b #066h,&P1SEL                                    ; P1.2 and P1.3 TA1/2 otions

                                             mov.w R4,#0C00H                                       ;Initial R4 
                                             mov.w #1024-1,&CCR0                                 ; PWM Period
                                             mov.w #OUTMOD_7,&TA0CCTL1              ; CCR1 reset/set
                                             mov.w R4,&TA0CCR1                              ; CCR1 PWM Duty Cycle
                                             mov.w #ID_2,&TA0CTL                                ;  ID_0 input clock

                                            mov.w #TASSEL_2+MC_1,&TA0CTL ; SMCLK, upmode

                                             mov.w #510,&CCR2 ; CCR2 PWM Duty Cycle

                                             bis.b #CCIE,&TACCTL1 ; SMCLK, upmode

;
                                              Mainloop bis.w #CPUOFF,SR ; CPU off
                                              nop ; Required only for debugger

 ;-------------------------------------------------------------------------------

TA0_ISR; ISR for TACCR0
;-------------------------------------------------------------------------------
                      mov.w  R4, CCR1                                    ; change PWM output value.

                      clr.w &TACTL                                         ; Clear Timer_A control registers

                      mov.w #384,&CCR1                              ; CCR1 PWM Duty Cycle

                      bis.b #CCIE ,&TACCTL1                       ; Exit LPM0 on reti

                      inc.w R4

                      cmp.w R4,#0FFFh 

                      jnz   Lp1

                     mov.w   #0C00h,R4

LP1               reti ;

;--------------------------------------------------------------------------------------------------

;Look Up Table  Start Address &0FFC0 .

data
0C00H: 1024
0C02H: 1023
0C04H: 1021
0C06H: 1025
0C08H: 1026
0C0AH: 1020
0C0CH: 1021
0C0EH: 1029
0C10H: 1025
0C12H: 1016
0C14H: 1025

.

0FFFh: 0000.

;-------------------------------------------- End of data.