This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AD转换不成功,各位帮帮忙

Other Parts Discussed in Thread: MSP430F149

#include <msp430f149.h>
#include "usart.h"
#include "delay.h"

#define uint unsigned int
#define  uchar unsigned char

void AD_init (void);
unsigned int i;
uchar value=0;
uchar rec;
int main(void)
{
WDTCTL = WDTPW + WDTHOLD;
AD_init();//AD初始化
usartInit();//串口初始化

do
  {
    IFG1 &= ~OFIFG;               //Reset OFIFG
    for(i = 0xff; i > 0; i--);
  }
  while((IFG1 & OFIFG));
  BCSCTL1 &= ~XT2OFF;
  BCSCTL2 |= SELM_2 + SELS;
  while(1)
  {
   /*
    if((IFG1 & URXIFG0))
    {
     rec = rdata();
    }*/
   P6OUT &= ~BIT5;//转换没完成,开发板LED灯亮
   while(!(ADC12IFG & BIT0));
    P6OUT |= BIT5;
   value = ADC12MEM0;
   delay_ms(10);
    if((IFG1 & UTXIFG0))
    {
     // sdata(rec);
      sdata(value);
      delay_ms(5);
    }
  }
   /*
  while((ADC12IFG & ADC12IV_ADC12IFG0))
    {
     value = ADC12MEM0;
     sdata(value);
    }*/
 
}
void AD_init (void)
{
  P6DIR = 0XFF;
  P6OUT = 0Xff;
  P6DIR &= ~BIT0;
  P6SEL &= ~BIT0;
  P6SEL |= 0X01;//通道A0
  ADC12CTL0 = SHT0_2 + MSC + REFON +REF2_5V;//自动转换参考电压2.5V
  ADC12CTL0 |= ADC12ON;
  ADC12CTL0 |= ENC;
  ADC12CTL0 |= ADC12SC;
  ADC12CTL1 |= SHP; 
  ADC12CTL1 |= CONSEQ_2;//单通道多次转换
  ADC12MCTL0 |=SREF_1 + INCH_0;
}

灯一直亮,标志位没有置位,转换一直不成功。