This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于LCD和GPIO引脚复用的问题

Other Parts Discussed in Thread: MSP430F417

专家,您好!

我使用的是MSP430F417,在之前的设计中,一直只用了S0-S19共20×4=80段,现在我需要用到S21来增加4段。按照datasheet所讲,只能通过LCDPx来设置引脚,但是LCDPx只能按下表设置。就是要么用S0-S19,要么就S0-S23都设置为LCD的引脚。这样的话就多占浪费了3个GPIO,而且现在那3个引脚我已经分配了其它功能,而且没有其它多余引脚了。

因此,我该怎么办?能不能只让S20做LCD引脚,让S21-S23作为IO口使用?

000 No multiplexed pins are LCD function

001 S0-S15 are LCD function

010 S0-S19 are LCD function

011 S0-S23 are LCD function

100 S0-S27 are LCD function

101 S0-S31 are LCD function

110 S0-S35 are LCD function

111 S0-S39 are LCD function