This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助:G2332的IIC要如何使用

在数据手册上和IAR的头文件寄存器地址都不一样

  • 你用的是什么IDE,IAR还是CCS?什么版本的?哪里不一样了?

  • 你好,

    我们有MSP430WARE工具,里面有IIC的例程,无需你从头开始自己写。

    C:\ti\msp430\MSPWare_3_20_00_37

    C:\ti\msp430\MSPWare_3_20_00_37\examples\devices\MSP430G2xx\MSP430G2xx3_Code_Examples

    /* --COPYRIGHT--,BSD_EX
    * Copyright (c) 2012, Texas Instruments Incorporated
    * All rights reserved.
    *
    * Redistribution and use in source and binary forms, with or without
    * modification, are permitted provided that the following conditions
    * are met:
    *
    * * Redistributions of source code must retain the above copyright
    * notice, this list of conditions and the following disclaimer.
    *
    * * Redistributions in binary form must reproduce the above copyright
    * notice, this list of conditions and the following disclaimer in the
    * documentation and/or other materials provided with the distribution.
    *
    * * Neither the name of Texas Instruments Incorporated nor the names of
    * its contributors may be used to endorse or promote products derived
    * from this software without specific prior written permission.
    *
    * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
    * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
    * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
    * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
    * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
    * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
    * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
    * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
    * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
    * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
    * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    *
    *******************************************************************************
    *
    * MSP430 CODE EXAMPLE DISCLAIMER
    *
    * MSP430 code examples are self-contained low-level programs that typically
    * demonstrate a single peripheral function or device feature in a highly
    * concise manner. For this the code may rely on the device's power-on default
    * register values and settings such as the clock configuration and care must
    * be taken when combining code from several examples to avoid potential side
    * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
    * for an API functional library-approach to peripheral configuration.
    *
    * --/COPYRIGHT--*/
    //******************************************************************************
    // MSP430G2xx2 Demo - I2C Slave Receiver, single byte
    //
    // Description: I2C Slave communicates with I2C Master using
    // the USI. Master data should increment from 0x00 with each transmitted byte
    // which is verified by the slave.
    // LED off for address or data Ack; LED on for address or data NAck.d by the slave.
    // ACLK = n/a, MCLK = SMCLK = Calibrated 1MHz
    //
    // ***THIS IS THE SLAVE CODE***
    //
    // Slave Master
    // (MSP430G2xx2_usi_07.c)
    // MSP430G2xx2 MSP430G2xx2
    // ----------------- -----------------
    // /|\| XIN|- /|\| XIN|-
    // | | | | | |
    // --|RST XOUT|- --|RST XOUT|-
    // | | | |
    // LED <-|P1.0 | | |
    // | | | P1.0|-> LED
    // | SDA/P1.7|<-------|P1.7/SDA |
    // | SCL/P1.6|<-------|P1.6/SCL |
    //
    // Note: internal pull-ups are used in this example for SDA & SCL
    //
    // D. Dang
    // Texas Instruments Inc.
    // December 2010
    // Built with CCS Version 4.2.0 and IAR Embedded Workbench Version: 5.10
    //******************************************************************************

    #include <msp430.h>


    char MST_Data = 0; // Variable for received data
    char SLV_Addr = 0x90; // Address is 0x48<<1 for R/W
    int I2C_State = 0; // State variable

    int main(void)
    {
    WDTCTL = WDTPW + WDTHOLD; // Stop watchdog
    if (CALBC1_1MHZ==0xFF) // If calibration constants erased
    {
    while(1); // do not load, trap CPU!!
    }

    DCOCTL = 0; // Select lowest DCOx and MODx settings
    BCSCTL1 = CALBC1_1MHZ; // Set DCO
    DCOCTL = CALDCO_1MHZ;

    P1OUT = 0xC0; // P1.6 & P1.7 Pullups
    P1REN |= 0xC0; // P1.6 & P1.7 Pullups
    P1DIR = 0xFF; // Unused pins as outputs
    P2OUT = 0;
    P2DIR = 0xFF;

    USICTL0 = USIPE6+USIPE7+USISWRST; // Port & USI mode setup
    USICTL1 = USII2C+USIIE+USISTTIE; // Enable I2C mode & USI interrupts
    USICKCTL = USICKPL; // Setup clock polarity
    USICNT |= USIIFGCC; // Disable automatic clear control
    USICTL0 &= ~USISWRST; // Enable USI
    USICTL1 &= ~USIIFG; // Clear pending flag
    __enable_interrupt();

    while(1)
    {
    LPM0; // CPU off, await USI interrupt
    __no_operation(); // Used for IAR
    }
    }

    //******************************************************************************
    // USI interrupt service routine
    //******************************************************************************
    #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
    #pragma vector = USI_VECTOR
    __interrupt void USI_TXRX (void)
    #elif defined(__GNUC__)
    void __attribute__ ((interrupt(USI_VECTOR))) USI_TXRX (void)
    #else
    #error Compiler not supported!
    #endif
    {
    if (USICTL1 & USISTTIFG) // Start entry?
    {
    P1OUT |= 0x01; // LED on: sequence start
    I2C_State = 2; // Enter 1st state on start
    }

    switch(I2C_State)
    {
    case 0: // Idle, should not get here
    break;

    case 2: // RX Address
    USICNT = (USICNT & 0xE0) + 0x08; // Bit counter = 8, RX address
    USICTL1 &= ~USISTTIFG; // Clear start flag
    I2C_State = 4; // Go to next state: check address
    break;

    case 4: // Process Address and send (N)Ack
    if (USISRL & 0x01) // If read...
    SLV_Addr++; // Save R/W bit
    USICTL0 |= USIOE; // SDA = output
    if (USISRL == SLV_Addr) // Address match?
    {
    USISRL = 0x00; // Send Ack
    P1OUT &= ~0x01; // LED off
    I2C_State = 8; // Go to next state: RX data
    }
    else
    {
    USISRL = 0xFF; // Send NAck
    P1OUT |= 0x01; // LED on: error
    I2C_State = 6; // Go to next state: prep for next Start
    }
    USICNT |= 0x01; // Bit counter = 1, send (N)Ack bit
    break;

    case 6: // Prep for Start condition
    USICTL0 &= ~USIOE; // SDA = input
    SLV_Addr = 0x90; // Reset slave address
    I2C_State = 0; // Reset state machine
    break;

    case 8: // Receive data byte
    USICTL0 &= ~USIOE; // SDA = input
    USICNT |= 0x08; // Bit counter = 8, RX data
    I2C_State = 10; // Go to next state: Test data and (N)Ack
    break;

    case 10:// Check Data & TX (N)Ack
    USICTL0 |= USIOE; // SDA = output
    if (USISRL == MST_Data) // If data valid...
    {
    USISRL = 0x00; // Send Ack
    MST_Data++; // Increment Master data
    P1OUT &= ~0x01; // LED off
    }
    else
    {
    USISRL = 0xFF; // Send NAck
    P1OUT |= 0x01; // LED on: error
    }
    USICNT |= 0x01; // Bit counter = 1, send (N)Ack bit
    I2C_State = 6; // Go to next state: prep for next Start
    break;
    }

    USICTL1 &= ~USIIFG; // Clear pending flags
    }

  • 感谢你回复!我的芯片正在调试中。