Flash of MSP430 value line series(such as G2553) can be programmed via MSP430Flasher.exe tool? if not, is there any simple tool to erase, program, and verify flash content? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可以的!
两线制或者四线制都是支持的。Flasher采用命令行的方式,可以用于程序的下载或者从Flash中读取代码。
详细命令见下面WiKi
processors.wiki.ti.com/.../MSP430_Flasher_-_Command_Line_Programmer