1、本人使用的是MSP430F5529,用的是第三方评估板。在设计中要使用430的USB模块,通过USB口从430向PC传送大量的数据。并且通过pC端编写MFC界面来对数据如何读取进行一系列设置。即一个双向的通讯过程
2、430所用的调试环境为IAR,电脑为XP SP2操作系统
3、正在设计的初级阶段
我想问的问题是所谓的usb的msc模式是不是只是通过usb口来对于大量数据的存取的,例如对片外flash/sd卡等。而我要完成自己的目的是不是应该用CDC模式
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、本人使用的是MSP430F5529,用的是第三方评估板。在设计中要使用430的USB模块,通过USB口从430向PC传送大量的数据。并且通过pC端编写MFC界面来对数据如何读取进行一系列设置。即一个双向的通讯过程
2、430所用的调试环境为IAR,电脑为XP SP2操作系统
3、正在设计的初级阶段
我想问的问题是所谓的usb的msc模式是不是只是通过usb口来对于大量数据的存取的,例如对片外flash/sd卡等。而我要完成自己的目的是不是应该用CDC模式
您的理解是正确的。
一般MSC类配合文件系统,常用来做文件存储,比如U盘和SD卡,PC可以直接访问USB device上的文件。
对于其他的应用场合,您可以采用HID或者CDC类,在速度和驱动上有些区别,具体您可以查阅