This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2133 FRAM读写问题

Other Parts Discussed in Thread: MSP430FR2311


#include "msp430.h"
//#include "msp430fr2311.h"
#include "spi.h"
#include "MyDef.h"


#define uint unsigned int
#define uchar unsigned char
#define ulong unsigned long;
#define MCLK_FREQ_MHZ 8 // MCLK = 8MHz


#define FRAM_TEST_START 0xFD00 //FF80h-FFFFh,0xFD00

void FRAMWrite(void);
void Init_GPIO();
void Software_Trim(); // Software Trim to get the best DCOFTRIM value
uchar UART_RX(void);
void FRAMRead (void);

unsigned char count = 0;
unsigned long *FRAM_write_ptr;
unsigned int data;

uchar Udata[10];
uchar Tdata[10];
uchar data_i=0;
uchar data_Full_falg=0;
uint Uval;


int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer

// Configure GPIO
Init_GPIO();

PM5CTL0 &= ~LOCKLPM5; // Disable the GPIO power-on default high-impedance mode
// to activate 1previously configured port settings
/*

__bis_SR_register(SCG0); // disable FLL
CSCTL3 |= SELREF__REFOCLK; // Set REFO as FLL reference source
CSCTL1 = DCOFTRIMEN_1 | DCOFTRIM0 | DCOFTRIM1 | DCORSEL_3;// DCOFTRIM=3, DCO Range = 8MHz
CSCTL2 = FLLD_0 + 243; // DCODIV = 8MHz
__delay_cycles(3);
__bic_SR_register(SCG0); // enable FLL
Software_Trim(); // Software Trim to get the best DCOFTRIM value

CSCTL4 = SELMS__DCOCLKDIV | SELA__REFOCLK; // set default REFO(~32768Hz) as ACLK source, ACLK = 32768Hz
// default DCODIV as MCLK and SMCLK source

// Configure UART pins
P1SEL0 |= BIT6 | BIT7; // set 2-UART pin as second function

// Configure UART
UCA0CTLW0 |= UCSWRST;
UCA0CTLW0 |= UCSSEL__SMCLK;

// Baud Rate calculation
// 8000000/(16*9600) = 52.083
// Fractional portion = 0.083
// User's Guide Table 17-4: UCBRSx = 0x49
// UCBRFx = int ( (52.083-52)*16) = 1
UCA0BRW_L = 52; // 8000000/16/9600
UCA0BRW_H = 0x00;
UCA0MCTLW = 0x4900 | UCOS16 | UCBRF1_L;

*/
// Configure UART pins
P1SEL0 |= BIT6 | BIT7; // set 2-UART pin as second function

// Configure UART
UCA0CTLW0 |= UCSWRST;
UCA0CTLW0 |= UCSSEL_1; // set ACLK as BRCLK

// Baud Rate calculation. Referred to UG 17.3.10
// (1) N=32768/4800=6.827
// (2) OS16=0, UCBRx=INT(N)=6
// (4) Fractional portion = 0.827. Refered to UG Table 17-4, UCBRSx=0xEE.
UCA0BR0 = 6; // INT(32768/4800)
UCA0BR1 = 0x00;
UCA0MCTLW = 0xEE00;

UCA0CTLW0 &= ~UCSWRST; // Initialize eUSCI
UCA0IE |= UCRXIE; // Enable USCI_A0 RX interrupt

//__bis_SR_register(LPM3_bits|GIE); // Enter LPM3, interrupts enabled
__bis_SR_register(GIE);
//__no_operation(); // For debugger

FRAM_write_ptr = (unsigned long *)FRAM_TEST_START;
init_def();
//FRAMRead();

while(1)
{

UART_RX();


}


}

void delay(uint val)
{
uint i;

for(i=0;i<val;i++);

}


void FRAMWrite (void)
{
unsigned int i=0;

SYSCFG0 = FRWPPW;
//SYSCFG0 &= ~PFWP;
//SYSCFG0 &= ~DFWP;
// delay(2000);
for (i = 0; i < CFG_PARA_SIZE; i++)
{
//delay(10);
*FRAM_write_ptr++ = cfg_para[i];
//delay(10);
}
SYSCFG0 = FRWPPW | PFWP;
//SYSCFG0 |= PFWP;
}

void FRAMRead (void)
{
unsigned int i=0;

SYSCFG0 = FRWPPW;
//SYSCFG0 &= ~PFWP;
//SYSCFG0 &= ~DFWP;
// delay(2000);
for (i = 0; i < CFG_PARA_SIZE; i++)
{

//delay(10);
cfg_para[i]=*FRAM_write_ptr++;
// delay(10);

}
SYSCFG0 = FRWPPW | PFWP;
//SYSCFG0 |= PFWP;

}


void sent_byte(uchar data)//发送一个字节数据
{
while(UCTXIFG==0);
UCA0TXBUF=data;
delay(3000);
}

void sent_EER(uchar val)
{
uchar i;

delay(5000);

Tdata[0]='E';
Tdata[1]='E';
Tdata[2]='R';
Tdata[3]=val;

for(i=0;i<4;i++)
sent_byte(Tdata[i]);

}

void sent_data(uint val)
{
uchar i;

delay(5000);

Tdata[0]=0xFF;
Tdata[1]=0xFF;
//Tdata[2]='R';
Tdata[3]=val/256;
Tdata[4]=val & 0x00FF;

Tdata[5]=0x0D;
Tdata[6]=0x0A;

for(i=0;i<7;i++)
sent_byte(Tdata[i]);

}


void Software_Trim()
{
unsigned int oldDcoTap = 0xffff;
unsigned int newDcoTap = 0xffff;
unsigned int newDcoDelta = 0xffff;
unsigned int bestDcoDelta = 0xffff;
unsigned int csCtl0Copy = 0;
unsigned int csCtl1Copy = 0;
unsigned int csCtl0Read = 0;
unsigned int csCtl1Read = 0;
unsigned int dcoFreqTrim = 3;
unsigned char endLoop = 0;

do
{
CSCTL0 = 0x100; // DCO Tap = 256
do
{
CSCTL7 &= ~DCOFFG; // Clear DCO fault flag
}while (CSCTL7 & DCOFFG); // Test DCO fault flag

__delay_cycles((unsigned int)3000 * MCLK_FREQ_MHZ);// Wait FLL lock status (FLLUNLOCK) to be stable
// Suggest to wait 24 cycles of divided FLL reference clock
while((CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1)) && ((CSCTL7 & DCOFFG) == 0));

csCtl0Read = CSCTL0; // Read CSCTL0
csCtl1Read = CSCTL1; // Read CSCTL1

oldDcoTap = newDcoTap; // Record DCOTAP value of last time
newDcoTap = csCtl0Read & 0x01ff; // Get DCOTAP value of this time
dcoFreqTrim = (csCtl1Read & 0x0070)>>4;// Get DCOFTRIM value

if(newDcoTap < 256) // DCOTAP < 256
{
newDcoDelta = 256 - newDcoTap; // Delta value between DCPTAP and 256
if((oldDcoTap != 0xffff) && (oldDcoTap >= 256)) // DCOTAP cross 256
endLoop = 1; // Stop while loop
else
{
dcoFreqTrim--;
CSCTL1 = (csCtl1Read & (~DCOFTRIM)) | (dcoFreqTrim<<4);
}
}
else // DCOTAP >= 256
{
newDcoDelta = newDcoTap - 256; // Delta value between DCPTAP and 256
if(oldDcoTap < 256) // DCOTAP cross 256
endLoop = 1; // Stop while loop
else
{
dcoFreqTrim++;
CSCTL1 = (csCtl1Read & (~DCOFTRIM)) | (dcoFreqTrim<<4);
}
}

if(newDcoDelta < bestDcoDelta) // Record DCOTAP closest to 256
{
csCtl0Copy = csCtl0Read;
csCtl1Copy = csCtl1Read;
bestDcoDelta = newDcoDelta;
}

}while(endLoop == 0); // Poll until endLoop == 1

CSCTL0 = csCtl0Copy; // Reload locked DCOTAP
CSCTL1 = csCtl1Copy; // Reload locked DCOFTRIM
while(CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1)); // Poll until FLL is locked
}


#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=EUSCI_A0_VECTOR
__interrupt void USCI_A0_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCI_A0_VECTOR))) USCI_A0_ISR (void)
#else
#error Compiler not supported!
#endif
{

switch(__even_in_range(UCA0IV,18))
{
case 0x00: // Vector 0: No interrupts
break;
case 0x02: // Vector 2: UCRXIFG
Udata[data_i++]=UCA0RXBUF;
if(data_i>6)
{
data_i=0;
data_Full_falg=1;
}
break;
case 0x04: // Vector 4: UCTXIFG
break;
case 0x06: // Vector 6: UCSTTIFG
break;
case 0x08: // Vector 8: UCTXCPTIFG
break;
default: break;
}

// sent_byte(Udata[0]);

}

uchar UART_RX(void)
{
if(data_Full_falg==1)
{
data_Full_falg=0;
if((Udata[0]==0x55) && (Udata[1]==0x55) && (Udata[5]==0x0D))
{
Uval=Udata[3]*256+Udata[4];
Tdata[2]=Udata[2];
switch(Udata[2])
{
case 0x00: //
cfg_para[0]= (unsigned long)Uval;
FRAMWrite();
FRAMRead();
sent_EER('0');
break;
case 0x80: //
sent_data((unsigned int)cfg_para[0]);
break;
case 0x01: //
cfg_para[1]= (unsigned long)Uval;
FRAMWrite();
FRAMRead();
sent_EER('0');
break;
case 0x81: //
sent_data((unsigned int)cfg_para[1]);
break;
case 0x02: //
sent_EER('0');
break;
case 0x82: //
break;
case 0x03: //
sent_EER('0');
break;
case 0x83: //
break;
case 0x04: //
sent_EER('0');
break;
case 0x84: //
break;
case 0x05: //
sent_EER('0');
break;
case 0x85: //
break;
default:
sent_EER('9');
break;
}
data_i=0;
return 1;
}
else
{
data_i=0;
return 0;
}

}
else
return 0;

}

void Init_GPIO()
{
P1DIR = 0xFF; P2DIR = 0xFF;
P1REN = 0xFF; P2REN = 0xFF;
P1OUT = 0x00; P2OUT = 0x00;
}