This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

用两个msp430g2553使用ccs里的spi例程通信时,发现单独运行master的程序,master也能产生接受中断

Other Parts Discussed in Thread: MSP430G2553

  • //******************************************************************************

    // MSP430G2xx3 Demo - USCI_A0, SPI 3-Wire Master Incremented Data

    //

    // Description: SPI master talks to SPI slave using 3-wire mode. Incrementing

    // data is sent by the master starting at 0x01. Received data is expected to

    // be same as the previous transmission. USCI RX ISR is used to handle

    // communication with the CPU, normally in LPM0. If high, P1.0 indicates

    // valid data reception.

    // ACLK = n/a, MCLK = SMCLK = DCO ~1.2MHz, BRCLK = SMCLK/2

    //

    // Use with SPI Slave Data Echo code example. If slave is in debug mode, P3.6

    // slave reset signal conflicts with slave's JTAG; to work around, use IAR's

    // "Release JTAG on Go" on slave device. If breakpoints are set in

    // slave RX ISR, master must stopped also to avoid overrunning slave

    // RXBUF.

    //

    // MSP430G2xx3

    // -----------------

    // /|\| XIN|-

    // | | |

    // --|RST XOUT|-

    // | |

    // | P1.2|-> Data Out (UCA0SIMO)

    // | |

    // LED <-|P1.0 P1.1|<- Data In (UCA0SOMI)

    // | |

    // Slave reset <-|P1.5 P1.4|-> Serial Clock Out (UCA0CLK)

    //

    //

    // D. Dang

    // Texas Instruments Inc.

    // February 2011

    // Built with CCS Version 4.2.0 and IAR Embedded Workbench Version: 5.10

    //******************************************************************************

    #include "msp430g2553.h"

    #include "delay.h"

    unsigned int i = 0 ;

    unsigned char MST_Data, SLV_Data;

    void main(void)

    {

    volatile unsigned int i;

    WDTCTL = WDTPW + WDTHOLD; // Stop watchdog timer

    P1OUT = 0x00; // P1 setup for LED & reset output

    P1DIR |= BIT0 + BIT5; //

    P1SEL = BIT1 + BIT2 + BIT4;

    P1SEL2 = BIT1 + BIT2 + BIT4;

    UCA0CTL0 |= UCCKPL + UCMSB + UCMST + UCSYNC; // 3-pin, 8-bit SPI master

    UCA0CTL1 |= UCSSEL_2; // SMCLK

    UCA0BR0 |= 0x02; // /2

    UCA0BR1 = 0; //

    UCA0MCTL = 0; // No modulation

    UCA0CTL1 &= ~UCSWRST; // **Initialize USCI state machine**

    IE2 |= UCA0RXIE; // Enable USCI0 RX interrupt

    P1OUT &= ~BIT5; // Now with SPI signals initialized,

    P1OUT |= BIT5; // reset slave

    __delay_cycles(75); // Wait for slave to initialize

    MST_Data = 0x01; // Initialize data values

    SLV_Data = 0x00;

    UCA0TXBUF = MST_Data; // Transmit first character

    __bis_SR_register(LPM0_bits + GIE); // CPU off, enable interrupts

    }

    // Test for valid RX and TX character

    #pragma vector=USCIAB0RX_VECTOR

    __interrupt void USCIA0RX_ISR(void)

    {

    volatile unsigned int i;

    while (!(IFG2 & UCA0TXIFG)); // USCI_A0 TX buffer ready?

    if (UCA0RXBUF == SLV_Data) // Test for correct character RX'd

    i++;

    if(i>100){

    i =0;

    P1OUT ^= BIT0;

    }

    // P1OUT |= BIT0; // If correct, light LED

    // else

    // P1OUT &= ~BIT0; // If incorrect, clear LED

    MST_Data++; // Increment master value

    SLV_Data++; // Increment expected slave value

    UCA0TXBUF = MST_Data; // Send next value

    __delay_cycles(50); // Add time between transmissions to

    } // make sure slave can keep up

  • 这是master的程序。

    本来因该是master发送数据给slave。slave将接受到的数据又传给master。

    但现在master和slave之间没任何连接。但master竟然能进入接收中断。

    并且

    if (UCA0RXBUF == SLV_Data)                // Test for correct character RX'd

    还能这一条判断为真。。

    不解。

  • 1.程序分析:打开了接受中断,因为CLK是主机发出的,故SPI的接受端会在CLK的上升沿往UCA0RXBUF 中搬数据,在程序中 SLV_Data = 0x00;,如果悬空状态有可能SOMI脚读到的数据就是0.故能进中断而且会判断IF为真。

    2.中断程序写简短一些,最好是读UCA0RXBUF将其赋值给一个变量,然后就返回,其余的操作放在主函数中。

  • 首先第一个数传出去肯定是master这边发送出去的,那么如果有中断函数会进中断进行发送发送因为RX与TX是共享一个中断源的。

  • IE2 |= UCA0RXIE;                          // Enable USCI0 RX interrupt

    只使能了RX中断。TX中断应该不会发生吧。

    刚才我示波器测了下 MI,和MO(因为这里是master) 两个脚。发现MI 脚一直是高电平。

    MO 脚是有波形的。

    然后断点在中断服务程序中。UCA0RXBUF 每次进中断值都是0xFF。

    每次进中断 都会 SLV_Data++;

    于是如果发生255次中断后 SLV_Data 就 = 255 了。

    if (UCA0RXBUF == SLV_Data)

    就能判断通过了。

    是不是这样?

  • 本来程序前面使用空格对齐的,好像是发表出来前面的空格自动被去掉了。

    刚才右重新把空格加上去了。结果发表出来行首还是没空格。。。。

    期待能改进中!

  • 这个不是论坛本身的原因,而是IAR里的格式和论坛的格式不一致。

  • 1.是的,所以在SPI通讯时要考虑一个简单的应答判断,如果MISO是拉高的,则可判断收到有些0xFF是从机断开的时候发生的

    2.为了确认你的推断,可以在断点调试中看SVL_DATA的值变化,或者用toggle GPIO的方法用示波器观察