This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp430单片机中增量式pid算法的C实现方法

  •  #include <stdio.h>
      #include<math.h>
      
      struct _pid {
       int pv; /*integer that contains the process value*/
       int sp; /*integer that contains the set point*/
       float integral;
       float pgain;
       float igain;
       float dgain;
       int deadband;
       int last_error;
      };
      
      struct _pid warm,*pid;
      int process_point, set_point,dead_band; 
      float p_gain, i_gain, d_gain, integral_val,new_integ;; 
      
      
      
      /*------------------------------------------------------------------------ 
      pid_init 
      
      DESCRIPTION This function initializes the pointers in the _pid structure 
      to the process variable and the setpoint. *pv and *sp are 
      integer pointers. 
      ------------------------------------------------------------------------*/ 
      void pid_init(struct _pid *warm, int process_point, int set_point)
      { 
       struct _pid *pid; 
       
       pid = warm; 
       pid->pv = process_point; 
       pid->sp = set_point; 
      } 
      
      
      /*------------------------------------------------------------------------ 
      pid_tune 
      
      DESCRIPTION Sets the proportional gain (p_gain), integral gain (i_gain), 
      derivitive gain (d_gain), and the dead band (dead_band) of 
      a pid control structure _pid. 
      ------------------------------------------------------------------------*/ 
      
      void pid_tune(struct _pid *pid, float p_gain, float i_gain, float d_gain, int dead_band) 
      { 
       pid->pgain = p_gain; 
       pid->igain = i_gain; 
       pid->dgain = d_gain; 
       pid->deadband = dead_band; 
       pid->integral= integral_val; 
       pid->last_error=0; 
      } 
      
      /*------------------------------------------------------------------------ 
      pid_setinteg 
      
      DESCRIPTION Set a new value for the integral term of the pid equation. 
      This is useful for setting the initial output of the 
      pid controller at start up. 
      ------------------------------------------------------------------------*/ 
      void pid_setinteg(struct _pid *pid,float new_integ)
      { 
       pid->integral = new_integ; 
       pid->last_error = 0; 
      } 
      
      /*------------------------------------------------------------------------ 
      pid_bumpless 
      
      DESCRIPTION Bumpless transfer algorithim. When suddenly changing 
      setpoints, or when restarting the PID equation after an 
      extended pause, the derivative of the equation can cause 
      a bump in the controller output. This function will help 
      smooth out that bump. The process value in *pv should 
      be the updated just before this function is used. 
      ------------------------------------------------------------------------*/ 
      void pid_bumpless(struct _pid *pid) 
      { 
      
       pid->last_error = (pid->sp)-(pid->pv); 
       
      } 
      
      /*------------------------------------------------------------------------ 
      pid_calc 
      
      DESCRIPTION Performs PID calculations for the _pid structure *a. This function uses the positional form of the pid equation, and incorporates an integral windup prevention algorithim. Rectangular integration is used, so this function must be repeated on a consistent time basis for accurate control. 
      
      RETURN VALUE The new output value for the pid loop. 
      
      USAGE #include "control.h"*/ 
      
      
      float pid_calc(struct _pid *pid)
      { 
       int err;
       float pterm, dterm, result, ferror; 
       
       err = (pid->sp) - (pid->pv); 
       if (abs(err) > pid->deadband) 
       { 
       ferror = (float) err; /*do integer to float conversion only once*/ 
       pterm = pid->pgain * ferror; 
       if (pterm > 100 || pterm < -100)
       {
       pid->integral = 0.0; 
       }
       else 
       { 
       pid->integral += pid->igain * ferror; 
       if (pid->integral > 100.0) 
       {
       pid->integral = 100.0; 
       }
       else if (pid->integral < 0.0) pid->integral = 0.0; 
       } 
       dterm = ((float)(err - pid->last_error)) * pid->dgain; 
       result = pterm + pid->integral + dterm; 
       } 
       else result = pid->integral; 
       pid->last_error = err; 
       return (result); 
      }
      
      
      void main(void)
      {
       float display_value;
       int count=0;
      
       pid = &warm;
      
      // printf("Enter the values of Process point, Set point, P gain, I gain, D gain \n");
      // scanf("%d%d%f%f%f", &process_point, &set_point, &p_gain, &i_gain, &d_gain);
      
      
      
       process_point = 30;
       set_point = 40;
       p_gain = (float)(5.2);
       i_gain = (float)(0.77);
       d_gain = (float)(0.18);
      
      
      
       dead_band = 2;
       integral_val =(float)(0.01);
      
      
       printf("The values of Process point, Set point, P gain, I gain, D gain \n");
       printf(" %6d %6d %4f %4f %4f\n", process_point, set_point, p_gain, i_gain, d_gain);
      
       printf("Enter the values of Process point\n");
      
       while(count<=20)
       {
      
      
      
       scanf("%d",&process_point);
      
       pid_init(&warm, process_point, set_point);
       pid_tune(&warm, p_gain,i_gain,d_gain,dead_band);
       pid_setinteg(&warm,0.0); //pid_setinteg(&warm,30.0);
      
       //Get input value for process point
       pid_bumpless(&warm);
      
       // how to display output
       display_value = pid_calc(&warm); 
       printf("%f\n", display_value); 
       //printf("\n%f%f%f%f",warm.pv,warm.sp,warm.igain,warm.dgain); 
       count++; 
       
       } 
      
      }
  • 请教一下这个代码在CCS上编译通过不了,对结构体变量的定义应如何书写呢?谢谢!