This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
MSP430f5524 的USB插入可以被唤醒吗?哪里有相关的资料呀?
不具备这样功能,可以在USB口添加USB连接识别芯片来检测是否有连接USB设备:
The features of the USB module include:
• Fully compliant with the USB 2.0 Full-speed specification
– Full-speed device (12 Mbps) with integrated USB transceiver (PHY)
– Up to eight input and eight output endpoints
– Supports control, interrupt, and bulk transfers
– Supports USB suspend, resume, and remote wakeup