This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IAR中程序make出错



你好,我刚安装了IAR编译器,然后新建工作区->工程->c main函数

#include "io430.h"
#include "io430G2231.h"

int main( void )
{
  unsigned int i;
  // Stop watchdog timer to prevent time out reset`
  WDTCTL = WDTPW + WDTHOLD;
  P1DIR |= BIT0; //设置端口方向
  while(1)
  {
    P1OUT ^= BIT0; //端口输出翻转
    for(i = 0; i < 5000; i++);
  }

}

编译出错
Building configuration: myTest - Debug
Updating build tree...
Linking
Warning[w60]: The entry point label "__program_start" was not found in any input file. The

image will not have an entry point.
Error[e46]: Undefined external "__program_start" referred in ?ABS_ENTRY_MOD (  )
Error while running Linker
 
Total number of errors: 1
Total number of warnings: 1

请问这是为什么啊?我该怎么改呢?谢谢!

  • 程序本身没有问题。

    该问题应该是IAR设置问题,具体设置如下:

    Project->Option->Linker->Config 勾选"Override default program"

    再选择"Defined by application"

  • 谢谢您,Peter,编译这样通过了。但是点击“download and debug”出现 Stack Warning:

    The stack plug-in failed to set a breakpoint on "main". The Stack window will not be able to

    display stack contents.(You can change this setting in the Tools->Options dialog box.)

    我假设这没有问题,点击继续,在Disassembly界面:

    000000    0000               ????

    IFG1:

    IFG1.NMIIFG:

    IFG1.OFIFG:

    IFG1.PORIFG:

    IFG1.RSTIFG... +1 symbols not displayed:

    000002    0000               ????

    000004    0000               ????

    000006    0000               ????

    000008    0000               ????

    00000A    0000               ????

    00000C    0000               ????

    00000E    0000               ????

    000010    0000               ????

    000012    0000               ????

    000014    0000               ????

    Debug log界面:

    Tue Aug 21, 2012 09:12:35: Download complete.

    Tue Aug 21, 2012 09:12:35: Loaded debugee: G:\IAR\Debug\Exe\myTest.d43

    Tue Aug 21, 2012 09:12:35: Target reset

    Tue Aug 21, 2012 09:12:37: Couldn't go to 'main'.

    继续执行,出现User error: Illegal opcode found on address 0x0

    请问这是我哪里设置错误了...

  • 谢谢您,Peter,编译这样通过了。但是点击“download and debug”出现 Stack Warning:

    The stack plug-in failed to set a breakpoint on "main". The Stack window will not be able to

    display stack contents.(You can change this setting in the Tools->Options dialog box.)

    我假设这没有问题,点击继续,在Disassembly界面:

    000000    0000               ????

    IFG1:

    IFG1.NMIIFG:

    IFG1.OFIFG:

    IFG1.PORIFG:

    IFG1.RSTIFG... +1 symbols not displayed:

    000002    0000               ????

    000004    0000               ????

    000006    0000               ????

    000008    0000               ????

    00000A    0000               ????

    00000C    0000               ????

    00000E    0000               ????

    000010    0000               ????

    000012    0000               ????

    000014    0000               ????

    Debug log界面:

    Tue Aug 21, 2012 09:12:35: Download complete.

    Tue Aug 21, 2012 09:12:35: Loaded debugee: G:\IAR\Debug\Exe\myTest.d43

    Tue Aug 21, 2012 09:12:35: Target reset

    Tue Aug 21, 2012 09:12:37: Couldn't go to 'main'.

    继续执行,出现User error: Illegal opcode found on address 0x0

    请问这是我哪里设置错误了...

  • Project->Options->linker->output->format; 选择 Debug information for c-SPY选项