This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
不明白您的意思,是写程序到MSP430F1612?
可以的,MSP430F1612的JTAG口RST/TMS/TDI/TDO/TCK/VCC/GND都引出到了TP1-TP7上
1612不能用于编程。会破坏JTAG的firmware
对,就是烧程序到仿真芯片MSP430F1612里。
是可以的!因为Jtag口都引出来了。供电正常,接口接出来,没有理由不可以
我从Jtag 拉了6根线出来分别接了TP2-TP7,用ccs下载程序,下不了
Error connecting to the target:
Unknown device
这个我也没有做过实验。您是通过外部的FET430UIF进行烧写??
为什么要这么做?
对,我是通过外部MSP-FET430UIF进行烧写的。
只是想试下能不能这样对它编程
如上图,我发现F1612是没有TEST/VPP脚的。难道是这个原因么。。。。
那怎么用给F1612烧程序的。拉出来的TP2-TP7 又有啥用
1.不是这个原因,JTAG口与GPIO复用的MCU才有TEST引脚,F1612的JTAG口引脚是独立的,没有TEST是正常的。
2.引出来的JTAG就是给F1612烧程序的,但是是给工厂烧F1612作为仿真器的程序用的,如果JTAG 的Security Fuse在出厂时被熔断了,那么后面就不能通过JTAG给F1612烧程序了