This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最近购买了一个ADS1x9xEVM评估板,编译源代码工程时,报在identifier "UPCS0" is undefined。
评估板的MCU为 ,MSP430f5529
报错文件为usb.c
BYTE USB_enable()
{
.....
if (USB_PLL_XT == 2)
{
USBPLLCTL = UPCS0 + UPFDEN + UPLLEN;// Select XT2 as Ref / Select PLL for USB / Discrim. on, enable PLL
}
else
{
USBPLLCTL = UPFDEN + UPLLEN; // Select XT1 as Ref / Select PLL for USB / Discrim. on, enable PLL
}
....
}
我搜索了一下在include的文件msp430f5529.h里面能够找到UPFDEN , UPLLEN的定义,但是找不到UPCS0定义。
请问该UPCS0需要怎么定义?或者是否需要哪个头文件?谢谢!
用最新的库移植下,或者换以前的库,新版本不支持这个函数了。看勘误说明或者更新说明
Version: 1.073
==========================================================================================
release Package 11.03.2013
==========================================================================================
11.03.2013 added DCOR to MSP430G2x55 devices
added 5xx style defintions for 2xx/4xx devices for TA0IV Register
fixed some typos in 5xx/6xx device with TimerA/B Interrupt vector definitions
10.02.2013 fixed size of Signature in FRAM Devices
==========================================================================================
release Package 31.01.2013
==========================================================================================
31.01.2013 added MSP430G2755, MSP430G2855, MSP430G2955
15.01.2013 changed defines to CapTouchIO from CapSenseIO to align with Users Guide
13.12.2012 Module name changed from RTC_CE to RTC_C
13.12.2012 CCS: Removed Legacy CCE V2 defines for Interrupt Vectors
14.11.2012 fixed missing UCA1 in FR57x3/7
14.11.2012 FR56xx: fixed typo in SYSRSTIV_MPUSEG defintions
replaced COMP_B with COMP_E
==========================================================================================
release Package 13.11.2012
==========================================================================================
24.10.2012 replaced define TBSSEL__TACLK with TBSSEL__TBCLK
ADC12B: fixed some Typos in ADC12 definitions (ADC10 was used before)
28.09.2012 USB devices: removed UPCS0 definition
非常感谢楼上两位的详细回答,我觉得楼上两位分析很有道理。我现在只想把程序编译过去,能够跟踪TI提供的样例程序,所以就想用老版本的库。请问要到哪里找老版本的库,如何替换?谢谢!
http://dl.21ic.com/download/msp430ware_users_guide-1_00_00_00-pdf-ic-96339.html
21ic有1.0版本的下载,你可以看看这个版本。