This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430中断程序在IAR中编译错误



我写了个MSP430小中断测试程序,源代码如下:
#include "io430.h"
#include "io430G2231.h"

int main( void )
{
  // Stop watchdog timer to prevent time out reset`
  WDTCTL = WDTPW + WDTHOLD;
  P1DIR |= BIT0; //设置端口方向
  P1OUT |= BIT0;
 
  P1DIR &= ~BIT3;
  P1IE |= BIT3;  //打开1.3中断
  P1IES |= BIT3; //中断方式,P1  Interrupt Edge Select
  _BIS_SR(GIE);  //开系统中断
  while(1);
}

#pragma vector=PORT1_VECTOR
___interrupt void PORT1_ISR(void)
{
  P1IE &= ~BIT3;  //关闭1.3中断
  if((P1IFG & BIT3) == BIT3)
    P1OUT ^= BIT0;
  P1IFG &= ~BIT3;
  P1IE |= BIT3; //打开1.3中断
}
编译出现错误:
main.c 
Warning[Pe223]: function "_BIS_SR" declared implicitly G:\IAR\ISR\main.c 14
Error[Pe077]: this declaration has no storage class or type specifier G:\IAR\ISR\main.c 19
Warning[Pe609]: this kind of pragma may not be used here G:\IAR\ISR\main.c 18
Error[Pe065]: expected a ";" G:\IAR\ISR\main.c 19
Warning[Pe012]: parsing restarts here after previous syntax error G:\IAR\ISR\main.c 27
Error while running C/C++ compiler

Done. 2 error(s), 3 warning(s)

我的中断服务程序的申明格式有没错误呢?上面程序该怎么修改呢?
谢谢!