This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F149 仅下载时高速晶振(8M)停振,其他时候正常

Other Parts Discussed in Thread: MSP430F149

帮同学做了个430的板子,焊接的时候先焊接了最小系统部分,但是无法下载(BSL)。下载时提示同步失败(synchronization failed)。

检查晶振,32.768KHz无误,但8M上停振。换晶振,8M上有振荡,但幅度较低(Vpp=500mV左右)。换负载电容(原先为22p),发现当去除电容时幅度最大(Vpp=1.5V左右),且振荡稳定,用手触摸引脚不会停振。

现下载,使用示波器监测下载时8M晶振振荡情况:在未开始下载时振荡正常,点击下载按钮后停振,然后下载器显示“同步失败”,之后又恢复振荡,像是很受控的感觉,不像是硬件问题的样子。此外,只有先将BSL下载器连接电脑,再接入板子的BSL口,才能振荡,其他情况下均不起振。

板子就是最基本的最小系统,晶振也很靠近单片机。

这是帮同学做的一个板子,自己对430软件并不熟悉。上网查找资料貌似和程序设置有关?检查程序XT2的确是打开的,且在另一个开发板上下载也是没问题的。又或者是芯片版本问题(使用另一个BSL下载器时显示“加载补丁失败”)?

望解答,谢谢!