This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
若果是单片下载的话,使用离线编程器:比如利尔达等等厂家生产的都可以。
多片下载的武汉鑫人达有,其他等公司也有做的,找下专门做仿真器和下载器厂家一般都可以的。
多谢各位了,我用的是TI的MSP-FET430UIF MSP430-USB的仿真器,程序调试是用的IAR软件,可批量生产得生成HEX文件给产生部。所以得有一款支持该仿真器的HEX下载程序软件。谢谢!
多谢各位了,我用的是TI的MSP-FET430UIF MSP430-USB的仿真器,程序调试是用的IAR软件,可批量生产得生成HEX文件给产生部。所以得有一款支持该仿真器的HEX下载程序软件。谢谢!
1.程序的下载器和仿真器是没有关系的,以人吃饭举个例子,仿真器就像是人在享受晚宴,不仅是吃饱饭,还要把整个吃饭的过程使用起来,程序下载器就像是平时饿慌了给一个馒头直接填饱肚子。
2.所以你使用的程序下载器不是仿真器决定的,而是IDE给出来的,按照你的说法就是IAR生成的,使用TI自己做的MSP-GANG或者第三方Elprotronic的GnagPro430都是可以进行量产时的程序下载的;
3.你是不是想知道仿真器烧程序是和程序下载器烧FLASH的硬件接口问题,用4-wire的JTAG和SBW模式都是可以的,也是这两种程序下载都支持的,硬件的引脚顺序下载其对应的说明文档就可以看到;
4.程序下载器的PC端软件在这两中程序下载器的网页上可以下载到;提供一个TI的网页入口,希望能够帮助到你: