This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432,FLASH DOWNLOAD问题

我想让程序在RAM中执行(DEBUG和脱机都是),编译的程序的地址是基于RAM地址,程序的头有一段汇编语言负责 复制程序到RAM 和 跳转PC,现在最大的问题是,我如何把程序烧到了FLASH中?(编译器中,我如何设置了ICF文件中的RAM地址,程序会自动烧到RAM地址中,无法自由烧写)

可能我表达的不是很清楚,最简单的一句话,我想通过XDS100把指定文件写到FLASH的指定地址,这样可以吗?