Other Parts Discussed in Thread: MSP430G2231, MSP430G2221

(1) ARM系统通知MCU上电或下电RFID/IC等,
(2) MCU通知ARM系统SIM卡已上电。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430G2231, MSP430G2221

(1) ARM系统通知MCU上电或下电RFID/IC等,
(2) MCU通知ARM系统SIM卡已上电。
Kyle wang 说:(1)只用一根SDA线可以吗? 还是需要一根SDAIN,一根SDAOUT?
不行!数据线是一条SDA,双向的,还需要一条CLK。这个可以去查看I2C协议;
Kyle wang 说:(2)没很搞明白Master/slave中的receive操作和Transmitter操作…请问的两种操作这里只用Master中的receive操作和Transmitter操作就可以接收吗?还是属于Master中的receive操作和Slave中的Transmitter操作
在7位地址后面有一个bit用于标识读或者写。您就当成一个主人在向奴隶征收租子,主人负责发号施令,奴隶跟着执行就行了。
因为MSP430可以作为master或者slave嘛,所以程序编写的时候肯定会不一样。所以如果您MSP430做主机,主要看Master 接收和发送部分就可以了。
Kyle wang 说:(3)看了很久Family User Guide中的I2C原理…还是没搞明白其初始化以及传输流程,感觉晕晕的,里面的示例代码全是汇编的…如果有C代码对照着看起来就好多了…有哪位可以帮我讲讲吗…
您好!在做I2C之前,先去研究I2C的协议。有中文版的。看完协议以后,MSP430的初始化,以及状态机就很简单了。
Kyle wang 说:(4)正常的程序流程是,先初始化I2C,然后程序进入while(1),然后根据USI中断进行数据的处理,这里我的问题是:a. 怎么去使I2C的状态在master/slave中的发送/接收状态变换?
查看第2条
Kyle wang 说:(5)I2C上的数据通过什么去获取?一次可以传几位啊?
一次8bit。建议您花时间看协议。
(1)我图中有I2C_SCL,应该就是您说所的CLK吧?
(2)大概有点明白,对我来说,MSP430就是跑程序的地方,肯定只要作为Master用来做接收(指令)和发送(指令)即可,无需用到slave。
(3)我百度了下I2C协议,状态机大概明白了,感谢您!就是对初始化以及众寄存器的使用上,还得总对照着头文件看,有时也会乱乱的...
另外,有新的问题求教:
(4)我如何知道slave在通过I2C传MSP430传数据呢?是不是一旦slave或master有给I2C发数据,就会有一个USI中断产生呢?
(5)我的slave和写数据地址是多少?是连接I2C_SDA这个引脚的地址吗?
(6)那怎么在一个状态机中同时控制Master的发送和传输啊?
建议楼主应该找个资料先好好搞清楚I2C的硬件结构,数据传输方式。这样对您的提问更有帮助。即使解答您上面所有问题,相信您还是得自己慢慢消化。
您好!谢谢你们的建议!我也有在看,但是还是不知道slave address是多少...求教...
另外,我想把各引脚的状态(用status记录)保存起来,以便下次开机的时候恢复,并且通知上层系统。是不是在status变化的时候,需要把status写入内存flash中才能固化保存呢?
下面是一个C语音的例程,可供参考:
//******************************************************************************
// MSP430G2x21/G2x31 Demo - I2C Master Receiver, single byte
//
// Description: I2C Master communicates with I2C Slave using
// the USI. Slave data should increment from 0x00 with each transmitted byte
// which is verified by the Master.
// LED off for address or data Ack; LED on for address or data NAck.
// ACLK = n/a, MCLK = SMCLK = Calibrated 1MHz
//
// ***THIS IS THE MASTER CODE***
//
// Slave Master
// (msp430g2x21_usi_09.c)
// MSP430G2x21/G2x31 MSP430G2x21/G2x31
// ----------------- -----------------
// /|\| XIN|- /|\| XIN|-
// | | | | | |
// --|RST XOUT|- --|RST XOUT|-
// | | | |
// LED <-|P1.0 | | |
// | | | P1.0|-> LED
// | SDA/P1.7|------->|P1.7/SDA |
// | SCL/P1.6|<-------|P1.6/SCL |
//
// Note: internal pull-ups are used in this example for SDA & SCL
//
// D. Dang
// Texas Instruments Inc.
// October 2010
// Built with CCS Version 4.2.0 and IAR Embedded Workbench Version: 5.10
//******************************************************************************
#include <msp430g2221.h>
char SLV_data = 0x00; // Variable for received data
char SLV_Addr = 0x91; // Address is 0x48 << 1 bit + 1 for Read
int I2C_State = 0; // State variable
void main(void)
{
volatile unsigned int i; // Use volatile to prevent removal
WDTCTL = WDTPW + WDTHOLD; // Stop watchdog
if (CALBC1_1MHZ ==0xFF || CALDCO_1MHZ == 0xFF)
{
while(1); // If calibration constants are erased
// do not load, trap CPU!!
}
BCSCTL1 = CALBC1_1MHZ; // Set DCO
DCOCTL = CALDCO_1MHZ;
P1OUT = 0xC0; // P1.6 & P1.7 Pullups
P1REN |= 0xC0; // P1.6 & P1.7 Pullups
P1DIR = 0xFF; // Unused pins as outputs
P2OUT = 0;
P2DIR = 0xFF;
USICTL0 = USIPE6+USIPE7+USIMST+USISWRST;// Port & USI mode setup
USICTL1 = USII2C+USIIE; // Enable I2C mode & USI interrupt
USICKCTL = USIDIV_3+USISSEL_2+USICKPL;// Setup USI clocks: SCL = SMCLK/8 (~120kHz)
USICNT |= USIIFGCC; // Disable automatic clear control
USICTL0 &= ~USISWRST; // Enable USI
USICTL1 &= ~USIIFG; // Clear pending flag
_EINT();
while(1)
{
USICTL1 |= USIIFG; // Set flag and start communication
LPM0; // CPU off, await USI interrupt
_NOP(); // Used for IAR
for (i = 0; i < 5000; i++); // Dummy delay between communication cycles
}
}
/******************************************************
// USI interrupt service routine
******************************************************/
#pragma vector = USI_VECTOR
__interrupt void USI_TXRX (void)
{
switch(I2C_State)
{
case 0: // Generate Start Condition & send address to slave
P1OUT |= 0x01; // LED on: sequence start
USISRL = 0x00; // Generate Start Condition...
USICTL0 |= USIGE+USIOE;
USICTL0 &= ~USIGE;
USISRL = SLV_Addr; // ... and transmit address, R/W = 1
USICNT = (USICNT & 0xE0) + 0x08; // Bit counter = 8, TX Address
I2C_State = 2; // Go to next state: receive address (N)Ack
break;
case 2: // Receive Address Ack/Nack bit
USICTL0 &= ~USIOE; // SDA = input
USICNT |= 0x01; // Bit counter = 1, receive (N)Ack bit
I2C_State = 4; // Go to next state: check (N)Ack
break;
case 4: // Process Address Ack/Nack & handle data RX
if (USISRL & 0x01) // If Nack received...
{ // Prep Stop Condition
USICTL0 |= USIOE;
USISRL = 0x00;
USICNT |= 0x01; // Bit counter = 1, SCL high, SDA low
I2C_State = 10; // Go to next state: generate Stop
P1OUT |= 0x01; // Turn on LED: error
}
else // Ack received
{ // Receive Data from slave
USICNT |= 0x08; // Bit counter = 8, RX data
I2C_State = 6; // Go to next state: Test data and (N)Ack
P1OUT &= ~0x01; // LED off
}
break;
case 6: // Send Data Ack/Nack bit
USICTL0 |= USIOE; // SDA = output
if (USISRL == SLV_data) // If data valid...
{
USISRL = 0x00; // Send Ack
SLV_data++; // Increment Slave data
P1OUT &= ~0x01; // LED off
}
else
{
USISRL = 0xFF; // Send NAck
P1OUT |= 0x01; // LED on: error
}
USICNT |= 0x01; // Bit counter = 1, send (N)Ack bit
I2C_State = 8; // Go to next state: prep stop
break;
case 8: // Prep Stop Condition
USICTL0 |= USIOE; // SDA = output
USISRL = 0x00;
USICNT |= 0x01; // Bit counter = 1, SCL high, SDA low
I2C_State = 10; // Go to next state: generate Stop
break;
case 10: // Generate Stop Condition
USISRL = 0x0FF; // USISRL = 1 to release SDA
USICTL0 |= USIGE; // Transparent latch enabled
USICTL0 &= ~(USIGE+USIOE);// Latch/SDA output disabled
I2C_State = 0; // Reset state machine for next transmission
LPM0_EXIT; // Exit active for next transfer
break;
}
USICTL1 &= ~USIIFG; // Clear pending flag
}
1.根据你的原理图是接的MCU的USI的IIC功能,如果使用USI配置成IIC使用,则SDA是主机从机共用数据线,除非是将其用作IO口模拟SPI总线用或者UART用则是需要一去一来两根数据线,当然从你提供的原理图和说明看,应该是当IIC总线用;
2.master transmitter -> slave receiver, master receiver <- slave transmitter, 就这两种模式
3.TI官网上有USI实现IIC的例程,可以下下来看看。
4.转换发送接收状态,设置USICTL0中USIOE置一则设置为输出-发送,置零则设置为输入-接收;
5.在成功握手后,如果数据发送到接收到完成接收(移位寄存器完成),则会置USIIFG位,进入中断读取USISRL的值,IIC协议一次传输8个bit数据。
Leon Yan提供了一段Master receiver的代码,这里是一段slave transmitter的代码,分别烧进两个MCU,
把两个MCU的IIC接口用线连起来就可以正常通讯了,用逻辑分析仪可以看到通讯时的波形
//******************************************************************************
// MSP430G2x21/G2x31 Demo - I2C Slave Transmitter, single byte
//
// Description: I2C Slave communicates with I2C Master using
// the USI. Slave data is sent and increments from 0x00 with each transmitted
// byte which is verified by the Master.
// LED off for address or data Ack; LED on for address or data NAck.
// ACLK = n/a, MCLK = SMCLK = Calibrated 1MHz
//
// ***THIS IS THE SLAVE CODE***
//
// Slave Master
// (msp430g2x21_usi_06.c)
// MSP430G2x21/G2x31 MSP430G2x21/G2x31
// ----------------- -----------------
// /|\| XIN|- /|\| XIN|-
// | | | | | |
// --|RST XOUT|- --|RST XOUT|-
// | | | |
// LED <-|P1.0 | | |
// | | | P1.0|-> LED
// | SDA/P1.7|------->|P1.7/SDA |
// | SCL/P1.6|<-------|P1.6/SCL |
//
// Note: internal pull-ups are used in this example for SDA & SCL
//
// D. Dang
// Texas Instruments Inc.
// October 2010
// Built with CCS Version 4.2.0 and IAR Embedded Workbench Version: 5.10
//******************************************************************************
#include <msp430g2221.h>
char SLV_Data = 0; // Variable for transmitted data
char SLV_Addr = 0x90; // Address is 0x48<<1 for R/W
int I2C_State = 0; // State variable
void main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Stop watchdog
if (CALBC1_1MHZ ==0xFF || CALDCO_1MHZ == 0xFF)
{
while(1); // If calibration constants erased
// do not load, trap CPU!!
}
BCSCTL1 = CALBC1_1MHZ; // Set DCO
DCOCTL = CALDCO_1MHZ;
P1OUT = 0xC0; // P1.6 & P1.7 Pullups
P1REN |= 0xC0; // P1.6 & P1.7 Pullups
P1DIR = 0xFF; // Unused pins as outputs
P2OUT = 0;
P2DIR = 0xFF;
USICTL0 = USIPE6+USIPE7+USISWRST; // Port & USI mode setup
USICTL1 = USII2C+USIIE+USISTTIE; // Enable I2C mode & USI interrupts
USICKCTL = USICKPL; // Setup clock polarity
USICNT |= USIIFGCC; // Disable automatic clear control
USICTL0 &= ~USISWRST; // Enable USI
USICTL1 &= ~USIIFG; // Clear pending flag
_EINT();
while(1)
{
LPM0; // CPU off, await USI interrupt
_NOP(); // Used for IAR
}
}
//******************************************************
// USI interrupt service routine
//******************************************************
#pragma vector = USI_VECTOR
__interrupt void USI_TXRX (void)
{
if (USICTL1 & USISTTIFG) // Start entry?
{
P1OUT |= 0x01; // LED on: Sequence start
I2C_State = 2; // Enter 1st state on start
}
switch(I2C_State)
{
case 0: //Idle, should not get here
break;
case 2: //RX Address
USICNT = (USICNT & 0xE0) + 0x08; // Bit counter = 8, RX Address
USICTL1 &= ~USISTTIFG; // Clear start flag
I2C_State = 4; // Go to next state: check address
break;
case 4: // Process Address and send (N)Ack
if (USISRL & 0x01) // If read...
SLV_Addr++; // Save R/W bit
USICTL0 |= USIOE; // SDA = output
if (USISRL == SLV_Addr) // Address match?
{
USISRL = 0x00; // Send Ack
P1OUT &= ~0x01; // LED off
I2C_State = 8; // Go to next state: TX data
}
else
{
USISRL = 0xFF; // Send NAck
P1OUT |= 0x01; // LED on: error
I2C_State = 6; // Go to next state: prep for next Start
}
USICNT |= 0x01; // Bit counter = 1, send (N)Ack bit
break;
case 6: // Prep for Start condition
USICTL0 &= ~USIOE; // SDA = input
SLV_Addr = 0x90; // Reset slave address
I2C_State = 0; // Reset state machine
break;
case 8: // Send Data byte
USICTL0 |= USIOE; // SDA = output
USISRL = SLV_Data; // Send data byte
USICNT |= 0x08; // Bit counter = 8, TX data
I2C_State = 10; // Go to next state: receive (N)Ack
break;
case 10:// Receive Data (N)Ack
USICTL0 &= ~USIOE; // SDA = input
USICNT |= 0x01; // Bit counter = 1, receive (N)Ack
I2C_State = 12; // Go to next state: check (N)Ack
break;
case 12:// Process Data Ack/NAck
if (USISRL & 0x01) // If Nack received...
{
P1OUT |= 0x01; // LED on: error
}
else // Ack received
{
P1OUT &= ~0x01; // LED off
SLV_Data++; // Increment Slave data
}
// Prep for Start condition
USICTL0 &= ~USIOE; // SDA = input
SLV_Addr = 0x90; // Reset slave address
I2C_State = 0; // Reset state machine
break;
}
USICTL1 &= ~USIIFG; // Clear pending flags
}
非常地感谢大家的热心解答!我已经大概明白其原理和流程了,再问一个问题:
我想实现:按键1.5按下时通过I2C发送Data给slave。并随时接收来自slave的I2C数据。数据都是1个byte的
那我如下程序是否可以用来实现上述功能。有哪里错误需要修改吗?
while(1)
{
// receive I2C Data
DataDirection = Receive;
USICTL1 |= USIIFG; // Set flag and start communication
LPM0; // CPU off, await USI interrupt
__no_operation();
for (i = 0; i < 5000; i++); // Dummy delay between communication cycles
}
#pragma vector=PORT1_VECTOR
__interrupt void PORT1_ISR(void)
{
P1IE &= ~BIT5; //disable 1.5 interrupt
if((P1IFG & BIT5) == BIT5)
{//send I2C Data
DataDirection = Transmit;
USICTL1 |= USIIFG; // Set flag and start communication
LPM0; // CPU off, await USI interrupt
__no_operation();
}
P1IE |= BIT5; //enable 1.5 interrupt
}
//下面是个I2C中断状态机控制,太长先不贴出来