最近在做一个便携式测量仪器产品,关机需要进入低功耗状态LPM4,但进入LPM4状态后发现整体功耗还是有近300uA。而基本上同样的电路,原先用的是MSP430F149就没有这么大的功耗,才20uA左右。
在进入LPM4之前,已经将未用的端口置为输出,且输出为0;端口连接有器件的,器件电源可关闭的也按前面的情况处理的;连接到端口的器件电源不能关闭的有三个,一个是SPI接口的大容量存储器,器件本身有指令可以进入低功耗状态(15uA);其它两个都是IIC接口的,一个是AT24C128-2.7V,另一个是时钟芯片RX-8025,在停止条件下的功耗都很低约6uA,因为有上拉电阻,所以进入LPM4前设置对应端口为输出高电平。
问题应该不在于外围电路,因为我将电源不受控的器件卸下了,整体功耗基本上没有什么改观,还是在300uA左右,所以怀疑是5418内部某些模块需要在进入LPM4之前进行处理,不知道专家有什么建议?谢谢!