This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all
我在做一个项目,需要用到RTC的低功耗模式 ,但我实测发现上电后的功耗是0.4uA,但执行完第一次中断程序后,之后不管进入多少次中断,进入RTC低功耗模式都是12.6uA。我试过和定时时间没关系,第一次中断前都是0.4uA。请问是我需要在每次再次进入低功耗时都需要重新配置下RTC吗?
// MSP430FR413x Demo - RTC, device enter LPM3.5 and toggle P1.0 in RTC interrupt handling every 1s // // // Description: Device enter LPM3.5 after configuring the RTC. The RTC wakes // the device up from LPM3.5 every second and toggles P1.0. // It also stores the state of P0OUT in the Backup RAM Registers. // // ACLK = XT1 = 32kHz, MCLK = SMCLK = default DCODIV = ~1MHz. // // MSP430FR4133 // ----------------- // /|\| | // | | | // | | XIN(P4.1)|-- // --|RST | ~32768Hz // | XOUT(P4.2)|-- // | | // | P4.5|-->LED // // Wei Zhao // Texas Instruments Inc. // March 2015 // Built with IAR Embedded Workbench v6.20 & Code Composer Studio v6.1 //****************************************************************************** #include <msp430.h> void initGpio(void); int main(void) { WDTCTL = WDTPW | WDTHOLD; // Stop WDT initGpio(); // Configure GPIO // Initialize XT1 32kHz crystal P4SEL0 |= BIT1 | BIT2; // set XT1 pin as second function do { CSCTL7 &= ~(XT1OFFG | DCOFFG); // Clear XT1 and DCO fault flag SFRIFG1 &= ~OFIFG; } while (SFRIFG1 & OFIFG); // Test oscillator fault flag // First determine whether we are coming out of an LPMx.5 or a regular RESET. if (SYSRSTIV == SYSRSTIV_LPM5WU) // When woken up from LPM3.5, reinit { // If MCU wakes up from LPM3.5, re-init and then return to LPM3.5 again. // Restore P1OUT value from backup RAM memory, keep P1OUT after LPMx.5 reset P4OUT = *(unsigned int *)BKMEM_BASE; __enable_interrupt(); // The RTC interrupt should trigger now... } else { // Device powered up from a cold start. // It configures the device and puts the device into LPM3.5 // Configure backup memory *(unsigned int *)BKMEM_BASE = 0; // Initialize RTC // Interrupt and reset happen every 1024/32768 * 32 = 1 sec. RTCMOD = 960-1; RTCCTL = RTCSS__XT1CLK | RTCSR | RTCPS__1024 | RTCIE; // Store P1OUT value in backup memory register before enter LPM3.5 *(unsigned int *)BKMEM_BASE = P4OUT; } // Enter LPM3.5 mode with interrupts enabled. Note that this operation does // not return. The LPM3.5 will exit through a RESET event, resulting in a // re-start of the code. PMMCTL0_H = PMMPW_H; // Open PMM Registers for write PMMCTL0_L |= PMMREGOFF; // and set PMMREGOFF __bis_SR_register(LPM3_bits | GIE); __no_operation(); return 0; } void initGpio(void) { P1DIR |= 0x1F; P2DIR |= 0xFF; P3DIR |= 0xFF; P4DIR |= 0xFF; P5DIR |= 0xFF; P6DIR |= 0xFF; P7DIR |= 0xFF; P8DIR |= 0xFD; P1OUT |= 0x1F; P2OUT |= 0xFF; P3OUT |= 0xFF; P3OUT &= ~0x87; P4OUT |= 0xFF; P5OUT |= 0xFF; P6OUT |= 0xFF; P7OUT |= 0xFF; P8OUT |= 0xFD; P8DIR &= ~0x02; P8REN &= ~0x02; //Motor P1.6 1.7 1.5 P1DIR &= ~0xE0; P1REN &= ~0xE0; P2DIR &= ~0xF3; P2REN &= ~0xF3; // Disable the GPIO power-on default high-impedance mode // to activate previously configured port settings PM5CTL0 &= ~LOCKLPM5; } #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__) #pragma vector = RTC_VECTOR __interrupt void RTC_ISR(void) #elif defined(__GNUC__) void __attribute__ ((interrupt(RTC_VECTOR))) RTC_ISR (void) #else #error Compiler not supported! #endif { switch(__even_in_range(RTCIV, RTCIV_RTCIF)) { case RTCIV_NONE : break; // No interrupt pending case RTCIV_RTCIF: // RTC Overflow // Toggle LED on P1.0 P4OUT ^= BIT5; // Store P1OUT value in backup memory register *(unsigned int *)BKMEM_BASE = P4OUT; __bis_SR_register(LPM3_bits | GIE); break; default: break; } }
yanqing zhou 说:Hi all
我在做一个项目,需要用到RTC的低功耗模式 ,但我实测发现上电后的功耗是0.4uA,但执行完第一次中断程序后,之后不管进入多少次中断,进入RTC低功耗模式都是12.6uA。我试过和定时时间没关系,第一次中断前都是0.4uA。请问是我需要在每次再次进入低功耗时都需要重新配置下RTC吗?
// MSP430FR413x Demo - RTC, device enter LPM3.5 and toggle P1.0 in RTC interrupt handling every 1s // // // Description: Device enter LPM3.5 after configuring the RTC. The RTC wakes // the device up from LPM3.5 every second and toggles P1.0. // It also stores the state of P0OUT in the Backup RAM Registers. // // ACLK = XT1 = 32kHz, MCLK = SMCLK = default DCODIV = ~1MHz. // // MSP430FR4133 // ----------------- // /|\| | // | | | // | | XIN(P4.1)|-- // --|RST | ~32768Hz // | XOUT(P4.2)|-- // | | // | P4.5|-->LED // // Wei Zhao // Texas Instruments Inc. // March 2015 // Built with IAR Embedded Workbench v6.20 & Code Composer Studio v6.1 //****************************************************************************** #include <msp430.h> void initGpio(void); int main(void) { WDTCTL = WDTPW | WDTHOLD; // Stop WDT initGpio(); // Configure GPIO // Initialize XT1 32kHz crystal P4SEL0 |= BIT1 | BIT2; // set XT1 pin as second function do { CSCTL7 &= ~(XT1OFFG | DCOFFG); // Clear XT1 and DCO fault flag SFRIFG1 &= ~OFIFG; } while (SFRIFG1 & OFIFG); // Test oscillator fault flag // First determine whether we are coming out of an LPMx.5 or a regular RESET. if (SYSRSTIV == SYSRSTIV_LPM5WU) // When woken up from LPM3.5, reinit { // If MCU wakes up from LPM3.5, re-init and then return to LPM3.5 again. // Restore P1OUT value from backup RAM memory, keep P1OUT after LPMx.5 reset P4OUT = *(unsigned int *)BKMEM_BASE; __enable_interrupt(); // The RTC interrupt should trigger now... } else { // Device powered up from a cold start. // It configures the device and puts the device into LPM3.5 // Configure backup memory *(unsigned int *)BKMEM_BASE = 0; // Initialize RTC // Interrupt and reset happen every 1024/32768 * 32 = 1 sec. RTCMOD = 960-1; RTCCTL = RTCSS__XT1CLK | RTCSR | RTCPS__1024 | RTCIE; // Store P1OUT value in backup memory register before enter LPM3.5 *(unsigned int *)BKMEM_BASE = P4OUT; } // Enter LPM3.5 mode with interrupts enabled. Note that this operation does // not return. The LPM3.5 will exit through a RESET event, resulting in a // re-start of the code. PMMCTL0_H = PMMPW_H; // Open PMM Registers for write PMMCTL0_L |= PMMREGOFF; // and set PMMREGOFF __bis_SR_register(LPM3_bits | GIE); __no_operation(); return 0; } void initGpio(void) { P1DIR |= 0x1F; P2DIR |= 0xFF; P3DIR |= 0xFF; P4DIR |= 0xFF; P5DIR |= 0xFF; P6DIR |= 0xFF; P7DIR |= 0xFF; P8DIR |= 0xFD; P1OUT |= 0x1F; P2OUT |= 0xFF; P3OUT |= 0xFF; P3OUT &= ~0x87; P4OUT |= 0xFF; P5OUT |= 0xFF; P6OUT |= 0xFF; P7OUT |= 0xFF; P8OUT |= 0xFD; P8DIR &= ~0x02; P8REN &= ~0x02; //Motor P1.6 1.7 1.5 P1DIR &= ~0xE0; P1REN &= ~0xE0; P2DIR &= ~0xF3; P2REN &= ~0xF3; // Disable the GPIO power-on default high-impedance mode // to activate previously configured port settings PM5CTL0 &= ~LOCKLPM5; } #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__) #pragma vector = RTC_VECTOR __interrupt void RTC_ISR(void) #elif defined(__GNUC__) void __attribute__ ((interrupt(RTC_VECTOR))) RTC_ISR (void) #else #error Compiler not supported! #endif { switch(__even_in_range(RTCIV, RTCIV_RTCIF)) { case RTCIV_NONE : break; // No interrupt pending case RTCIV_RTCIF: // RTC Overflow // Toggle LED on P1.0 P4OUT ^= BIT5; // Store P1OUT value in backup memory register *(unsigned int *)BKMEM_BASE = P4OUT; __bis_SR_register(LPM3_bits | GIE); break; default: break; } }
LPM3.5功耗是比较低,但是从LPM3.5唤醒之后需要做一些初始化,这段时间比较耗电,如果应用唤醒频率不是很低的话建议用 LPM3. 操作简单,功耗也低。