This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS7.1 编译工程提示找不到文件。是不是软件安装的不正确,安装是32位的软件,系统是WIN10 64 位的系统



下面是console 提示


**** Clean-only build of configuration Debug for project Lab05-2_Captouch ****

"E:\\Program Files\\ccs7.1\\ccsv7\\utils\\bin\\gmake" -k clean
DEL /F "Lab05-2_Captouch.out"
DEL /F "dr_lcdseg.obj" "main.obj"
DEL /F "dr_lcdseg.d" "main.d"
找不到 D:\project\mcu\MCU430\Labs_v02\Lab05-2_Captouch\Debug\Lab05-2_Captouch.out
找不到 D:\project\mcu\MCU430\Labs_v02\Lab05-2_Captouch\Debug\dr_lcdseg.obj
找不到 D:\project\mcu\MCU430\Labs_v02\Lab05-2_Captouch\Debug\dr_lcdseg.d
'Finished clean'
' '

**** Build Finished ****
Buildfile generation error occurred..
This project was created using a version of compiler that is not currently installed: 4.0.0 [MSP430]. See 'Help > Check for Updates' or visit CCS App Center to get the latest compilers. See 'Help > Install New Software...' to install older compilers. Alternatively, migrate the project to one of the available compiler versions by adjusting project properties.
Build stopped..