您好!
我在做MSP430F5529LP与MSP430F5529 POCKET KIT中的电子墨水屏实验中,遇到如下问题:
能将初始化程序中电子墨水屏上显示内容擦除,但无法重新调用display函数。目前还未发现问题出在哪里,请教论坛上的朋友。
谢谢!
/****************************main文件************************************/
#include <msp430.h> #include "Paper_Display.h" #define TimesNewRoman 0 #define Arial 1 #define ArialBlack 2 #define size8 0 #define size16 1 volatile unsigned char DisBuffer[250*16]; void initClock() { UCSCTL6 &= ~XT1OFF; //启动XT1 P5SEL |= BIT2 + BIT3; //XT2引脚功能选择 UCSCTL6 &= ~XT2OFF; //打开XT2 __bis_SR_register(SCG0); UCSCTL0 = DCO0+DCO1+DCO2+DCO3+DCO4; UCSCTL1 = DCORSEL_4; //DCO频率范围在28.2MHZ以下 UCSCTL2 = FLLD_5 + 1; //D=16,N=1 UCSCTL3 = SELREF_5 + FLLREFDIV_3; //n=8,FLLREFCLK时钟源为XT2CLK;DCOCLK=D*(N+1)*(FLLREFCLK/n);DCOCLKDIV=(N+1)*(FLLREFCLK/n); UCSCTL4 = SELA_4 + SELS_3 +SELM_3; //ACLK的时钟源为DCOCLKDIV,MCLK\SMCLK的时钟源为DCOCLK UCSCTL5 = DIVA_5 +DIVS_1; //ACLK由DCOCLKDIV的32分频得到,SMCLK由DCOCLK的2分频得到 //最终MCLK:16MHZ,SMCLK:8MHZ,ACLK:32KHZ // __bic_SR_register(SCG0); //Enable the FLL control loop } int main(void) { int i=180; WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer P8DIR |= BIT1; P8OUT &=~ BIT1; initClock(); PaperIO_Int(); INIT_SSD1673(); Init_buff(); display("Hello", 42, 0,TimesNewRoman,size8,1,0); display("E-INK", 42, 16,TimesNewRoman,size8,0,0); while(1) { } }
/****************************Paper_Display.h文件************************************/
#include <msp430.h>
#define nRST_H P1OUT|=BIT4
#define nRST_L P1OUT&=~BIT4
#define nCS_H P3OUT|=BIT2
#define nCS_L P3OUT&=~BIT2
#define SDA_H P3OUT|=BIT3
#define SDA_L P3OUT&=~BIT3
#define SCLK_H P2OUT|=BIT7
#define SCLK_L P2OUT&=~BIT7
#define nDC_H P3OUT|=BIT4
#define nDC_L P3OUT&=~BIT4
#define nBUSY P2IN & BIT2
extern volatile unsigned char DisBuffer[250*16];
void SPI4W_WRITECOM(unsigned char INIT_COM);
void SPI4W_WRITEDATA(unsigned char INIT_DATA);
void SPI4W_WRITE(unsigned char INIT_COM,unsigned char INIT_DATA);
void MYRESET(void);
void WRITE_LUT(void);
void INIT_SSD1673(void);
void DIS_IMG(unsigned char num);
void FIRST_PICTURE(void);
void IMAGE_WRITE(unsigned char patt_num);
void DELAY_100nS(unsigned int delaytime);
void DELAY_mS(unsigned int delaytime);
void DELAY_S(unsigned int delaytime);
void DELAY_M(unsigned int delaytime);
void RING(void);
void READBUSY(void);
void closebump(void);
void DisplayString(const char* str, unsigned int sx, unsigned int sy);
void enterdeepsleep(void);
void Init_buff(void);
void SET_EYEONE(void);
void PaperIO_Int(void);
void display(unsigned char *str, //字符串
unsigned int xsize, //x方向位置
unsigned int ysize, //y方向位置
unsigned int font, //字体 0,1,2
unsigned int size, //字号 0,1
unsigned int reverse,//反显 0 正常显示, 1 反显
unsigned int fresh //立即刷新
);
/****************************Paper_Display.c文件************************************/
#include <msp430.h>
#include "Include.h"
#include "Paper_Display.h"
#define DELAY_TIME 50 // 图片显示完停留时间(单位:秒)
// 测试图
#define PIC_WHITE 255 // 全白
#define PIC_BLACK 254 // 全黑
#define PIC_Orientation 253 // 方向图
#define PIC_LEFT_BLACK_RIGHT_WHITE 249 // 左黑右白
#define PIC_UP_BLACK_DOWN_WHITE 248 // 上黑下白
const unsigned char init_data[]={
0x50,0xAA,0x55,0xAA,0x55,0xAA,0x11,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x0F,0x0F,0x0F,0x0F,
0x0F,0x0F,0x0F,0x01,0x00,0x00,0x00,0x00,0x00,
};
void MyRESET()
{
nRST_L;
DELAY_mS(10);//1ms
nRST_H;
DELAY_mS(10);//1ms
}
void DELAY_100nS(unsigned int delaytime) // 30us
{
int i,j;
for(i=0;i<delaytime;i++)
for(j=0;j<10;j++);
}
void DELAY_mS(unsigned int delaytime) // 1ms
{
int i;
for(i=0;i<delaytime;i++)
__delay_cycles(200);
}
void DELAY_S(unsigned int delaytime) // 1s
{
int i;
for(i=0;i<delaytime;i++)
{
__delay_cycles(3276);
}
}
void DELAY_M(unsigned int delaytime) // 1M
{
int i;
for(i=0;i<delaytime;i++)
DELAY_S(60);
}
void READBUSY()
{
while(1)
{ //=1 BUSY
if((P2IN & BIT2)==0)
break;
}
DELAY_M(2);
}
void FIRST_PICTURE()
{
SPI4W_WRITECOM(0x21);
SPI4W_WRITEDATA(0x83);
SPI4W_WRITECOM(0x22);
SPI4W_WRITEDATA(0xC4);
}
void INIT_SSD1673()
{
MyRESET();
READBUSY();
SPI4W_WRITECOM(0x01); // Gate Setting
SPI4W_WRITEDATA(0xF9); // MUX Gate lines=250-1=249(F9H)
SPI4W_WRITEDATA(0x00); // B[2]:GD=0[POR](G0 is the 1st gate output channel) B[1]:SM=0[POR](left and right gate interlaced) B[0]:TB=0[POR](scan from G0 to G319)
SPI4W_WRITECOM(0x3A); // number of dummy line period set dummy line for 50Hz frame freq
SPI4W_WRITEDATA(0x06); // Set 50Hz A[6:0]=06h[POR] Number of dummy line period in term of TGate
SPI4W_WRITECOM(0x3B); // Gate line width set gate line for 50Hz frame freq
SPI4W_WRITEDATA(0x0B); // A[3:0]=1011(78us) Line width in us 78us*(250+6)=19968us=19.968ms
SPI4W_WRITECOM(0x3C); // Select border waveform for VBD
// SPI4W_WRITEDATA(0x30); // GS0-->GS0
// SPI4W_WRITEDATA(0x31); // GS0-->GS1
// SPI4W_WRITEDATA(0x32); // GS1-->GS0
SPI4W_WRITEDATA(0x33); // GS1-->GS1 开机第一次刷新Border从白到白
// SPI4W_WRITEDATA(0x43); // VBD-->VSS
// SPI4W_WRITEDATA(0x53); // VBD-->VSH
// SPI4W_WRITEDATA(0x63); // VBD-->VSL
// SPI4W_WRITEDATA(0x73); // VBD-->HiZ
SPI4W_WRITECOM(0x11); // Data Entry mode
SPI4W_WRITEDATA(0x01); // 01 –Y decrement, X increment
SPI4W_WRITECOM(0x44); // set RAM x address start/end, in page 22
SPI4W_WRITEDATA(0x00); // RAM x address start at 00h;
SPI4W_WRITEDATA(0x0f); // RAM x address end at 0fh(15+1)*8->128 2D13
SPI4W_WRITECOM(0x45); // set RAM y address start/end, in page 22
SPI4W_WRITEDATA(0xF9); // RAM y address start at FAh-1; 2D13
SPI4W_WRITEDATA(0x00); // RAM y address end at 00h; 2D13
SPI4W_WRITECOM(0x2C); // Vcom= *(-0.02)+0.01???
// SPI4W_WRITEDATA(0x82); //-2.5V
// SPI4W_WRITEDATA(0x69); //-2V
SPI4W_WRITEDATA(0x4B); //-1.4V
// SPI4W_WRITEDATA(0x50); //-1.5V
// SPI4W_WRITEDATA(0x37); //-1V
// SPI4W_WRITEDATA(0x1E); //-0.5V
WRITE_LUT();
SPI4W_WRITECOM(0x21); // Option for Display Update
SPI4W_WRITEDATA(0x83); // A[7]=1(Enable bypass) A[4]=0全黑(value will be used as for bypass)
DIS_IMG(PIC_WHITE); // 全黑到全白清屏,这样可防止开机出现花屏的问题
SPI4W_WRITECOM(0x21); //
SPI4W_WRITEDATA(0x03); // 后面刷新恢复正常的前后2幅图比较
SPI4W_WRITECOM(0x3C); // Select border waveform for VBD
SPI4W_WRITEDATA(0x73); // VBD-->HiZ 后面刷新时Border都是高阻
}
void WRITE_LUT()
{
unsigned char i;
SPI4W_WRITECOM(0x32);//write LUT register
for(i=0;i<29;i++)
SPI4W_WRITEDATA(init_data[i]);//write LUT register
}
void Init_buff(void)
{
int i;
for(i=0;i<4000;i++)
{
DisBuffer[i]=gImage_logo[i];
}
}
//xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx
//xx 图片显示函数 xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx
//xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx
void DIS_IMG(unsigned char num)
{
unsigned int row, col;
unsigned int pcnt;
SPI4W_WRITECOM(0x4E);
SPI4W_WRITEDATA(0x00); // set RAM x address count to 0;
SPI4W_WRITECOM(0x4F);
SPI4W_WRITEDATA(0xF9); // set RAM y address count to 250-1; 2D13
DELAY_S(5);
SPI4W_WRITECOM(0x24);
DELAY_S(5);
pcnt = 0; // 复位或保存提示字节序号
for(col=0; col<250; col++) // 总共250 GATE列 // send 128x250bits ram 2D13
{
for(row=0; row<16; row++) // 总共128 SOURCE行,每个像素1bit,即 128/8=16 字节
{
switch (num)
{
case 1:
SPI4W_WRITEDATA(DisBuffer[pcnt]);
break;
case 2:
SPI4W_WRITEDATA(gImage_logo[pcnt]);
break;
case PIC_WHITE:
SPI4W_WRITEDATA(0xff);
break;
default:
break;
}
pcnt++;
}
}
SPI4W_WRITECOM(0x22);
SPI4W_WRITEDATA(0xC7); // (Enable Clock Signal, Enable CP) (Display update,Disable CP,Disable Clock Signal)
// SPI4W_WRITEDATA(0xF7); // (Enable Clock Signal, Enable CP, Load Temperature value, Load LUT) (Display update,Disable CP,Disable Clock Signal)
SPI4W_WRITECOM(0x20);
DELAY_mS(1);
READBUSY();
DELAY_S(DELAY_TIME);
}
void SetpointXY(unsigned int xs,unsigned int xe,unsigned int ys,unsigned int ye)
{
SPI4W_WRITECOM(0x44);//set RAM x address start/end, in page 36
SPI4W_WRITEDATA(xs);//RAM x address start at 00h;
SPI4W_WRITEDATA(xe);//RAM x address end at 11h(17)->72: [because 1F(31)->128 and 12(18)->76]
SPI4W_WRITECOM(0x45);//set RAM y address start/end, in page 37
SPI4W_WRITEDATA(ys);//RAM y address start at 00h;
SPI4W_WRITEDATA(ye);//RAM y address start at ABh(171)->172: [because B3(179)->180]
SPI4W_WRITECOM(0x4E);//set RAM x address count to 0;
SPI4W_WRITEDATA(xs);
SPI4W_WRITECOM(0x4F);//set RAM y address count to 0;
SPI4W_WRITEDATA(ye);
SPI4W_WRITECOM(0x24);
}
void enterdeepsleep()
{
SPI4W_WRITECOM(0x10);
SPI4W_WRITEDATA(0x01);
}
void SPI4W_WRITECOM(unsigned char INIT_COM)
{
unsigned char TEMPCOM;
unsigned char scnt;
TEMPCOM=INIT_COM;
nCS_H;
nCS_L;
SCLK_L;
nDC_L;
for(scnt=0;scnt<8;scnt++)
{
if(TEMPCOM&0x80)
SDA_H;
else
SDA_L;
DELAY_100nS(10);
SCLK_H;
DELAY_100nS(10);
SCLK_L;
TEMPCOM=TEMPCOM<<1;
DELAY_100nS(10);
}
nCS_H;
}
void SPI4W_WRITEDATA(unsigned char INIT_DATA)
{
unsigned char TEMPCOM;
unsigned char scnt;
TEMPCOM=INIT_DATA;
nCS_H;
nCS_L;
SCLK_L;
nDC_H;
for(scnt=0;scnt<8;scnt++)
{
if(TEMPCOM&0x80)
SDA_H;
else
SDA_L;
DELAY_100nS(10);
SCLK_H;
DELAY_100nS(10);
SCLK_L;
TEMPCOM=TEMPCOM<<1;
DELAY_100nS(10);
}
nCS_H;
}
unsigned char FontSize[]={16,32};
void display(unsigned char *str, //字符串
unsigned int xsize, //x方向位置
unsigned int ysize, //y方向位置
unsigned int font, //字体 0,1,2
unsigned int size, //字号 0,1
unsigned int reverse,//反显 0 正常显示, 1 反显
unsigned int fresh //立即刷新
)
{
unsigned char i,j,k;
unsigned char *zimoPoint;
unsigned char zimoW;
unsigned char zimoH;
unsigned char moveBytes; //移动字节数
unsigned char moveBits; //移动位数
volatile unsigned char zimoBufferTemp[6];
zimoW=FontSize[size]/2; //x向行数
zimoH=FontSize[size]/8; //y向字节数
moveBits=ysize%8;
if((moveBits)!=0) //非完整字节处理
{
moveBytes=zimoH+1;
}
else moveBytes=zimoH;
while(*str)
{
if((font==TimesNewRoman) && (size==size8)) zimoPoint=(unsigned char *)&TimesNewRoman8;
else if((font==TimesNewRoman) && (size==size16)) zimoPoint=(unsigned char *)&TimesNewRoman16;
zimoPoint=zimoPoint+((*str)-0x20)*zimoW*zimoH; //指向字符字模的开始地址。
for(i=0;i<zimoW;i++)
{
//读出字模一列数据
for(j=0;j<6;j++) zimoBufferTemp[j]=0;
if(reverse==0)
{
for(j=0;j<zimoH;j++)
{
zimoBufferTemp[j]=~(*(zimoPoint+i+j*zimoW));
}
}
else
{
for(j=0;j<zimoH;j++)
{
zimoBufferTemp[j]=(*(zimoPoint+i+j*zimoW));
}
}
//字模一列数据移位操作
if (moveBits==0);
else
{
for(k=0;k<moveBits;k++)
{
for(j=moveBytes;j>0;j--)
{
zimoBufferTemp[j]=zimoBufferTemp[j]>>1;
if ((zimoBufferTemp[j-1]&0x01)>0) zimoBufferTemp[j]=zimoBufferTemp[j]+0x80;
}
zimoBufferTemp[0]=zimoBufferTemp[0]>>1;
}
}
//DisBuffer处理
if (moveBits==0);
else
{
k=(0xff>>moveBits);
zimoBufferTemp[moveBytes-1]=zimoBufferTemp[moveBytes-1] | (DisBuffer[(xsize+i)*16+((ysize/8)+zimoH)] & k);
k=~k;
zimoBufferTemp[0]=zimoBufferTemp[0] | (DisBuffer[(xsize+i)*16+(ysize/8)] & k);
}
//更新 DisBuffer
for(j=0;j<moveBytes;j++)
{
DisBuffer[(xsize+i)*16+((ysize/8)+j)]=zimoBufferTemp[j];
}
}
xsize=xsize+zimoW;
str++;
}
}
void PaperIO_Int(void)
{
P1DIR |= BIT4;
P2DIR |= BIT7;
P2DIR &= ~BIT2;
P3DIR |= BIT2 + BIT3 + BIT4;
}