This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

单片机跑死,无法复位,请求技术援助! 附上上了电路设计图,多谢各位高手帮忙!

Other Parts Discussed in Thread: TPS62110, MSP430F5310

我在单片机上烧好程序,让其运行。我是加了看门狗,也有低功耗LPM3模式。

具体运行环境是这样的:单片机初始化完成后进入低功耗LPM3,手动按键或定时开机退出低功耗,并打开看门狗(ACLK时钟源,1s定时),我是在程序的主函数while(1)中喂狗的(加了指示灯闪烁,能看到是否在喂狗);程序一直运行正常,喂狗指示灯闪烁,按键能控制单片机工作。但经过一天后单片机就不知道进入什么状态了,现象表现:1、喂狗指示灯没有闪烁; 2、按键中断不生效,或根本就没有进入按键中断(按键中断开始也加了指示灯的闪烁),指示灯没有亮;3、复位引脚手动拉低电平也不能使单片机复位(检测到了低电平信号进入单片机);4、此时检测外部供电3.3V正常,晶振正常,按键中断也有电平变化,但单片机就是死在那了。

当重新断电上电后又能正常工作了,这是什么状态啊?

请帮忙解决一下,时间紧迫,谢谢了!

电路使用环境:直流供电12V转3.3V(ti公司的TPS62110转换芯片转换的),测试时很稳定的。连接到430的AVCC1脚,再经过滤波后给DVCC1脚

附件是硬件设计图