This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于使用MSP430F67641平台的问题



有客户反馈使用http://www.ti.com/lit/zip/slaa621 这里面的计量库代码时(电表未进行任何校准工作),电表可以正确地读到电网的频率是50Hz左右,但是在只给A(B)(C)相电压的情况下,使用rms_voltage(0)(1)(2)读回来的电压都为0,给5A电流的情况下可以读到电流值为9.93A,使用active_power(0)读回来的功率为0,但是脉冲灯常亮,不产生脉冲。如果使用错误的电压线接法,如电压线接到A和C而不是A和地,可以看到脉冲灯闪烁这样奇怪的现象,但是功率读回来是0。
主要问题描述如下:
1)附件图1是只加电压调试时的图片,频率是正常,电压值和功率值不正常。
2)附件图2正常接法加5A电流时的图片,可以看出未校表时电流为9.9A,频率为50hz。电压和功率都不是正常的值。
3)附件图3错误接法,电压接AC,电流接A相,走5A电流的图片。电压值和上面图1、图2两个图不一样,不再是0x7FFFFF,变成0了。
4)附件图4是系统在运行一段时间后,电压值发生变化如下图
      因为项目比较紧急,客户对于该计量库的使用可能理解不够深刻,导致电表不能正常计量,希望能够得到相关技术的指导进行计量库的使用指导,针对上述问题进行解答,谢谢。
调试图片.rar