This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

不是说CCStudio 的编译器只能编译16K吗? 为何我的代码已经超过了, 还能编译和下载呢?

问题1: CCS代码限制为16K, 这个代码是指RAM的尺寸 还是 包括FRAM的尺寸?

因为我看我的代码有: 

MSP430: Flash/FRAM usage is 19670 bytes. RAM usage is 845 bytes.

这不是已经超过16K限制了吗? 为何还能编译和写进去? 难道TI已经在7.0版本去掉了限制?