This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS7.1版本安装问题

Other Parts Discussed in Thread: MSP430FR2633

在论坛中进行了安装问题的搜索,但是没有找到解决ccs7.1安装问题。

具体问题为:

1、An internal error occurred during: "CrashTrackerJob". Could not initialize class com.ti.utility.filesystem.DirectoryService$SingletonHolder

2、An internal error occurred during: "Loading device information". Could not initialize class com.ti.utility.filesystem.DirectoryService$SingletonHolder

3、This project was created for a device not currently supported: MSP430FR2633. See 'Help > Check for Updates' or visit <a href="liveaction:OpenAppCenter">CCS App Center</a> to get the latest device support. Alternatively, migrate the project to closest matching supported device by adjusting project properties.

问题3:我自己在app center 找了半天都没有看到最新的设备支持,还是没有解决这个问题

  • 你好,请看下wiki中关于Missing MSVC redistributable libraries部分,根据您的操作系统安装相应的Microsoft runtime libraries,望对你有帮助。

    http://processors.wiki.ti.com/index.php/Troubleshooting_CCSv7?keyMatch=CrashTrackerJob&tisearch=Search-EN-Everything

  • 从提示信息上看,应该是安装时由于错误或者有部分没完成安装,导致不能加载设备信息,所以提示不支持你的msp430型号。

    建议把ccs卸载删除干净后重新安装。安装ccs 时,一定要把杀毒软件、安全卫士等彻底关闭。

    不要使用阉割版的操作系统,不要使用家庭版操作系统

  • 参考你发给我的链接,下载并且安装了微软的一些库,但是还是出现了 An error has occurred.see  the log file C:\Users\Administrator\AppData\Local\Temp\ccs_c8ea7795-bb68-4dcd-4441-83840a38b1d1\workspace\.metadata\.log的错误,并且这个错误是在软件安装一半的时候出现的,出现这个错误以后软件就提示说安装完成,说明安装应该没有完成。

  • 你好,请问你的这个问题解决了吗?我也是这样的问题,安装了好几次都是同样的问题。。。期待你的回答。。谢谢

  • 这个问题一般都是安装时的问题,安装前注意先检查下杀毒软件是否还在后台运行
    不要使用国内各类ghost版的操作系统