Other Parts Discussed in Thread: MSP430FR5969
实例代码:
// MSP430F59xx Demo - eUSCI_A0, SPI 3-Wire Master Incremented Data
//
// Description: SPI master talks to SPI slave using 3-wire mode. Incrementing
// data is sent by the master starting at 0x01. Received data is expected to
// be same as the previous transmission TXData = RXData-1.
// USCI RX ISR is used to handle communication with the CPU, normally in LPM0.
// ACLK = 32.768kHz, MCLK = SMCLK = DCO ~1MHz. BRCLK = ACLK/2
//
//
// MSP430FR5969
// -----------------
// /|\ | XIN|-
// | | | 32KHz Crystal
// ---|RST XOUT|-
// | |
// | P2.0|-> Data Out (UCA0SIMO)
// | |
// | P2.1|<- Data In (UCA0SOMI)
// | |
// | P1.5|-> Serial Clock Out (UCA0CLK)
//
// P. Thanigai
// Texas Instruments Inc.
// Feb 2012
// Built with CCS V5.5
//******************************************************************************
#include <msp430.h>
volatile unsigned char RXData = 0;
volatile unsigned char TXData;
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
// Configure GPIO
P1SEL1 |= BIT5; // USCI_A0 operation
P2SEL1 |= BIT0 | BIT1; // USCI_A0 operation
PJSEL0 |= BIT4 | BIT5; // For XT1
// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5;
// XT1 Setup
CSCTL0_H = CSKEY >> 8; // Unlock CS registers
CSCTL1 = DCOFSEL_0; // Set DCO to 1MHz
CSCTL2 = SELA__LFXTCLK | SELS__DCOCLK | SELM__DCOCLK;
CSCTL3 = DIVA__1 | DIVS__1 | DIVM__1; // set all dividers
CSCTL4 &= ~LFXTOFF;
do
{
CSCTL5 &= ~LFXTOFFG; // Clear XT1 fault flag
SFRIFG1 &= ~OFIFG;
}while (SFRIFG1&OFIFG); // Test oscillator fault flag
CSCTL0_H = 0; // Lock CS registers
// Configure USCI_A0 for SPI operation
UCA0CTLW0 = UCSWRST; // **Put state machine in reset**
UCA0CTLW0 |= UCMST | UCSYNC | UCCKPL | UCMSB; // 3-pin, 8-bit SPI master
// Clock polarity high, MSB
UCA0CTLW0 |= UCSSEL__ACLK; // ACLK
UCA0BR0 = 0x02; // /2
UCA0BR1 = 0; //
UCA0MCTLW = 0; // No modulation
UCA0CTLW0 &= ~UCSWRST; // **Initialize USCI state machine**
UCA0IE |= UCRXIE; // Enable USCI_A0 RX interrupt
TXData = 0x1; // Holds TX data
while(1)
{
UCA0IE |= UCTXIE;
__bis_SR_register(LPM0_bits | GIE); // CPU off, enable interrupts
__delay_cycles(2000); // Delay before next transmission
TXData++; // Increment transmit data
}
}
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USCI_A0_VECTOR
__interrupt void USCI_A0_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCI_A0_VECTOR))) USCI_A0_ISR (void)
#else
#error Compiler not supported!
#endif
{
switch(__even_in_range(UCA0IV, USCI_SPI_UCTXIFG))
{
case USCI_NONE: break;
case USCI_SPI_UCRXIFG:
RXData = UCA0RXBUF;
UCA0IFG &= ~UCRXIFG;
__bic_SR_register_on_exit(LPM0_bits); // Wake up to setup next TX
break;
case USCI_SPI_UCTXIFG:
UCA0TXBUF = TXData; // Transmit characters
UCA0IE &= ~UCTXIE;
break;
default: break;
}
}
分析:直接分析SPI部分,其实这篇的话也是对我自己一些不理解的进行提问,希望能得到解答。这系列可以说是虎头蛇尾吧,不好意思。
1、配置USCI_A0为I2C模式。
(1)在配置或者重新配置eUSCI_A模块时应该先将UCSWRST置1以避免出现配置错误,配置完之后释放复位。
UCA0CTLW0 = UCSWRST; // **Put state machine in reset**
UCA0CTLW0 &= ~UCSWRST; // **Initialize USCI state machine**
(2)设置模式。
UCA0CTLW0 |= UCMST | UCSYNC | UCCKPL | UCMSB; // 3-pin, 8-bit SPI master
// Clock polarity high, MSB
其中,UCMST = 0x0800, UCSYNC = 0x0100, UCCKPL = 0x4000, UCMSB = 0x2000。
这里我们会发现,eUSCI_A在UART和SPI两种模式下,UCAxCTLW0 寄存器是不一样的。我有一个疑问:
eUSCI_A在UART和SPI两种模式是通过哪里切换的,只要PxSEL设置了两个引脚就是UART模式,四个引脚就自动进入SPI模式?
(3)选择eUSCI_A时钟源
UCA0CTLW0 |= UCSSEL__ACLK; // ACLK
其中,UCSSEL__ACLK = 0x0040。
(4)设置设置比特率。
UCA0BR0 = 0x02; // /2
UCA0BR1 = 0; //
fBitClock = fBRCLK/UCBRx
(5)我在SPI的模式说明里发现没有对UCA0MCTLW这个寄存器的说明,是不是和UART模式时的寄存器一模一样。用来配置波特率参数?希望有知道的帮忙解答下这条代码的作用:
UCA0MCTLW = 0; // No modulation
(6)使能中断
UCA0IE |= UCRXIE; // Enable USCI_A0 RX interrupt
2、处理函数(参考UART和I2C,这里不详述)
3、对于中断子程序(参考UART和I2C,这里不详述)