This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于MSp432捕获口驱动电流的求助

遇到一个问题,希望路过的大神多多指点:
我配置P10.4输出PWm脉冲串,将该信号接至P8.1进行上升与下降沿的捕获。分别使用库函数对这两个口进行配置。配置后,P10.4的脉冲是正常的,但是脉冲的高电平只有0.95V。通过库函数将P8.1配置为上拉电阻的(使用:extern void GPIO_setAsInputPinWithPullUpResistor(uint_fast8_t selectedPort,uint_fast16_t selectedPins);),P10.4脉冲的高电平上升至1.9V左右。我将P8.1的捕获功能禁止,P10.4的脉冲高电平上升至3.3V。
请问,配置成捕获功能的口,需要很大的驱动电流吗(我没找到捕获口驱动电流的资料)?就上述陈述的现象,需要在配置上拉电阻的同时在外接一个上拉电阻吗?谢谢