This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP4301611内部12位DAC模块如何消除输出的偏移误差

手册上写通过控制位DAC12CALON位可以校正,但在实际使用过程中发现仍然有偏移误差,常为负偏移0.01mv左右。

1.请问一下应该如何消除?

2.之前曾通过两路DA输出接差分运放的方式来消除,但由于差分运放放大倍数的限制使用受限,能否直接减小单片机DA输出的误差?

  • 你好:

            不知道你的输出电压范围是多大?在满足输出电压范围的要求下尽量减小参考电压。可以牺牲输出带宽提高输出精度。同时可以采用高精度高稳定性的外部参考电压。如果还不行,可以多次测量查看偏移量是否稳定在-0.01mV附近,如果是可以在软件中直接矫正。

  • 恩,我用的是内部2.5电源作为正参考电压,负参考电压就是AVss。测量的范围是从0.02V到2V,想的是用单片机内部的参考电压可以准一下。直接校正的方法我试一下,谢谢啦。