This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp430fr4133 launchpad 串口



请问你们的串口程序测试过吗?可以用吗?为什么用你们的板子和官方提供的程序,串口不能正常工作吗?开发环境是iar,其中一个程序如下

#include <msp430.h>
void Init_GPIO();
int main(void)
{
  WDTCTL = WDTPW | WDTHOLD;                // Stop watchdog timer
  // Configure GPIO
  Init_GPIO();
  PM5CTL0 &= ~LOCKLPM5;                    // Disable the GPIO power-on default high-impedance mode
                                           // to activate 1previously configured port settings
  __bis_SR_register(SCG0);                 // disable FLL
  CSCTL3 |= SELREF__REFOCLK;               // Set REFO as FLL reference source
  CSCTL0 = 0;                              // clear DCO and MOD registers
  CSCTL1 &= ~(DCORSEL_7);                  // Clear DCO frequency select bits first
  CSCTL1 |= DCORSEL_3;                     // Set DCO = 8MHz
  CSCTL2 = FLLD_0 + 243;                   // DCODIV = 8MHz
  __delay_cycles(3);
  __bic_SR_register(SCG0);                 // enable FLL
  while(CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1)); // Poll until FLL is locked
  CSCTL4 = SELMS__DCOCLKDIV | SELA__REFOCLK; // set default REFO(~32768Hz) as ACLK source, ACLK = 32768Hz
                                           // default DCODIV as MCLK and SMCLK source
  // Configure UART pins
  P1SEL0 |= BIT0 | BIT1;                    // set 2-UART pin as second function
  // Configure UART
  UCA0CTLW0 |= UCSWRST;
  UCA0CTLW0 |= UCSSEL__SMCLK;
 
  // Baud Rate calculation
  // 8000000/(16*9600) = 52.083
  // Fractional portion = 0.083
  // User's Guide Table 14-4: UCBRSx = 0x49
  // UCBRFx = int ( (52.083-52)*16) = 1
  UCA0BR0 = 52;                             // 8000000/16/9600
  UCA0BR1 = 0x00;
  UCA0MCTLW = 0x4900 | UCOS16 | UCBRF_1;
  UCA0CTLW0 &= ~UCSWRST;                    // Initialize eUSCI
  UCA0IE |= UCRXIE;                         // Enable USCI_A0 RX interrupt
  __bis_SR_register(LPM3_bits|GIE);         // Enter LPM3, interrupts enabled
  __no_operation();                         // For debugger
}
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USCI_A0_VECTOR
__interrupt void USCI_A0_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCI_A0_VECTOR))) USCI_A0_ISR (void)
#else
#error Compiler not supported!
#endif
{
  switch(__even_in_range(UCA0IV,USCI_UART_UCTXCPTIFG))
  {
    case USCI_NONE: break;
    case USCI_UART_UCRXIFG:
      while(!(UCA0IFG&UCTXIFG));
      UCA0TXBUF = UCA0RXBUF;
      __no_operation();
      break;
    case USCI_UART_UCTXIFG: break;
    case USCI_UART_UCSTTIFG: break;
    case USCI_UART_UCTXCPTIFG: break;
    default: break;
  }
}
void Init_GPIO()
{
    P1DIR = 0xFF; P2DIR = 0xFF; P3DIR = 0xFF; P4DIR = 0xFF;
    P5DIR = 0xFF; P6DIR = 0xFF; P7DIR = 0xFF; P8DIR = 0xFF;
    P1REN = 0xFF; P2REN = 0xFF; P3REN = 0xFF; P4REN = 0xFF;
    P5REN = 0xFF; P6REN = 0xFF; P7REN = 0xFF; P8REN = 0xFF;
    P1OUT = 0x00; P2OUT = 0x00; P3OUT = 0x00; P4OUT = 0x00;
    P5OUT = 0x00; P6OUT = 0x00; P7OUT = 0x00; P8OUT = 0x00;
}
没法工作啊!求解