This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
MSP430FR6972的PJ.0-3四个脚做GPIO时最大能提供多大的电流?
想用GPIO直接控制一片EEPROM的电源,最大要3mA的电流,不知道行不行?
有些msp430有提供6mA电流的io,但你用的这款手册上没说有这种io。
只在5.1 Absolute Maximum Ratings(1)部分提到:Diode current at any device pin 是正负2mA