This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5产生PWM,定时器溢出消除,尖峰脉冲

430单片机产生SPWM波,设定TA0CCR0为625,产生大概100个PWM时,也就是定时器的0XFFFF 65536时会产生一个占空比为1或者为0的PWM波,是因为定时器溢出,产生尖峰脉冲啥的吗,不懂,有没有大佬知道咋解决的嘛,感谢感谢

  • qian cheng2 说:

    430单片机产生SPWM波,设定TA0CCR0为625,产生大概100个PWM时,也就是定时器的0XFFFF 65536时会产生一个占空比为1或者为0的PWM波,是因为定时器溢出,产生尖峰脉冲啥的吗,不懂,有没有大佬知道咋解决的嘛,感谢感谢

    请把问题描述清楚。你想实现什么,遇到了什么问题?

  • 能否上传下你的程序?觉得你配置的可能不对。

    或者你参考下官网的例程

    //*******************************************************************************
    //  MSP430F552x Demo - Timer1_A3, PWM TA1.1-2, Up/Down Mode, 32kHz ACLK
    //
    //  Description: This program generates two PWM outputs on P2.0, P2.1 using
    //  Timer1_A configured for up/down mode. The value in CCR0, 128, defines the
    //  PWM period/2 and the values in CCR1 and CCR2 the PWM duty cycles. Using
    //  32kHz ACLK as TACLK, the timer period is 7.8ms with a 75% duty cycle
    //  on P2.0 and 25% on P2.1. Normal operating mode is LPM3
    //  ACLK = TACLK = LFXT1 = 32768Hz, MCLK = default DCO ~1.045MHz.
    //
    //                MSP430F552x
    //            -------------------
    //        /|\|                   |
    //         | |                   |
    //         --|RST                |
    //           |                   |
    //           |         P2.0/TA1.1|--> CCR1 - 75% PWM
    //           |         P2.1/TA1.2|--> CCR2 - 25% PWM
    //
    //   Bhargavi Nisarga
    //   Texas Instruments Inc.
    //   April 2009
    //   Built with CCSv4 and IAR Embedded Workbench Version: 4.21
    //******************************************************************************
    
    #include <msp430.h>
    
    int main(void)
    {
      WDTCTL = WDTPW + WDTHOLD;                 // Stop WDT
      P2DIR |= BIT0+BIT1;                       // P2.0 and P2.1 output
      P2SEL |= BIT0+BIT1;                       // P2.0 and P2.1 options select
      TA1CCR0 = 128;                            // PWM Period/2
      TA1CCTL1 = OUTMOD_6;                      // CCR1 toggle/set
      TA1CCR1 = 32;                             // CCR1 PWM duty cycle
      TA1CCTL2 = OUTMOD_6;                      // CCR2 toggle/set
      TA1CCR2 = 96;                             // CCR2 PWM duty cycle
      TA1CTL = TASSEL_1 + MC_3;                 // ACLK, up-down mode
    
      __bis_SR_register(LPM3_bits);             // Enter LPM3
      __no_operation();                         // For debugger
    }