如题,多谢……
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
USCI_A0, UART 9600 Full-Duplex Transceiver, 32K ACLK
int main(void)
{
WDTCTL = WDTPW+WDTHOLD; // Stop watchdog timer
P7SEL |= 0x03; // Port select XT1
do
{
UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + DCOFFG);
// Clear XT2,XT1,DCO fault flags
SFRIFG1 &= ~OFIFG; // Clear fault flags
__delay_cycles(100000); // Delay for Osc to stabilize
}while (SFRIFG1&OFIFG); // Test oscillator fault flag
P1OUT = 0x000; // P1.0/1 setup for LED output
P1DIR |= BIT0+BIT1; //
P3SEL |= BIT4+BIT5; // P3.4,5 UART option select
UCA0CTL1 |= UCSWRST; // **Put state machine in reset**
UCA0CTL1 |= UCSSEL_1; // CLK = ACLK
UCA0BR0 = 0x03; // 32k/9600 - 3.41
UCA0BR1 = 0x00; //
UCA0MCTL = 0x06; // Modulation
UCA0CTL1 &= ~UCSWRST; // **Initialize USCI state machine**
UCA0IE |= UCTXIE + UCRXIE; // Enable USCI_A0 TX/RX interrupt
}
希望能帮到你