This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于MSP430FR2633电容触摸防水功能的设计

我采MSP430FR2633做触摸按键,使用的是自感模式,请问在硬件上我需要怎么去实现防水功能?

  • Liu Zeng 说:

    我采MSP430FR2633做触摸按键,使用的是自感模式,请问在硬件上我需要怎么去实现防水功能?

    用 guard channel

    http://software-dl.ti.com/msp430/msp430_public_sw/mcu/msp430/CapTIvate_Design_Center/latest/exports/docs/users_guide/html/CapTIvate_Technology_Guide_html/markdown/ch_design_guide.html#moisture 

    Design Tips for Moisture Tolerance

    When designing a moisture tolerant application:

    1. Provide as much spacing as possible between buttons
    2. Provide significant spacing between buttons and nearby ground planes
    3. Route all electrode connection traces on the PCB layer furthest from the surface
    4. Set sensor idle states to High-Z (floating) so that nearby sensors don’t provide coupling points that can cause false detections
    5. If possible, use a non-conductive enclosure for the product

    Spill Rejection Applications

    Spill rejection applications include those which are able to detect when a fluid spill has occurred on the sensing panel. Common applications are white goods such as a cooking surface control panel. The goal of spill rejection is not to enable full touch detection (which is extremely difficult when moisture or fluids cover multiple keys and/or ground), but simply to detect the presence of a spill and lock out the keypad until the spill is cleared by a user. This is most commonly achieved with the use of a guard channel, whose purpose is to detect large objects as well as spills.

    Design Tips for Spill Detection

    When designing a spill detection application:

    1. Implement a guard channel to detect when a large unknown object or some kind of spill comes into contact with the sensing panel
    2. In software, utilize the guard channel to mask reporting of touches on other keys when a spill is detected.

    The CAPTIVATE-PHONE demonstration panel has a guard channel that is used for proximity sensing, palm rejection, and basic moisture rejection.