This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用ccs6.1开发MSP432 怎么设置CCS6.1可以在创建新工程时使用带库的模板



求大神解答 谢谢

  • 最简单的办法就是导入一个带库的例程,然后修改编写自己的程序

  • 还有 一个问题, 我在做官方给的通过GPIO PORT1中断控制DCO频率,改变led1的闪烁频率例程的时候,按了按键以后频率不改变,好像我的程序就进不了中断,但是我查看寄存器 我的P1IE寄存器已经使能了,我连续做了两个关于GPIO PORT1中断的实验都不成功。

    CS_initClockSignal(CS_MCLK,CS_DCOCLK_SELECT,CS_CLOCK_DIVIDER_1);这个代码中的三个参数,在cs.h中的#define 宏定义和在msp432p401r.h中的不一致,我改一直以后还是不行

    #define CS_CLOCK_DIVIDER_1          CS_CTL1_DIVS_0                #define CS_CTL1_DIVS_0                           ((uint32_t)0x00000000)          

    #define CS_MCLK          CS_CLKEN_MCLK_EN                                 #define CS_CLKEN_MCLK_EN                         ((uint32_t)0x00000002)

    #define CS_CLOCK_DIVIDER_1          CS_CTL1_DIVS_0               #define CS_CTL1_DIVS_0                           ((uint32_t)0x00000000)          

    大神给看看对么

  • 大神 能给我讲一下怎么使用MSP432的端口中断的问题么 谢谢