msp430f1232串口初始化的函数,主时钟8M,波特率9600
求一个函数例子
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
#include <msp430.h>
int main(void)
{
volatile unsigned int i;
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
P3SEL |= 0x30; // P3.4,5 = USART0 TXD/RXD
BCSCTL1 |= XTS; // ACLK = LFXT1 = HF XTAL
do
{
IFG1 &= ~OFIFG; // Clear OSCFault flag
for (i = 0xFF; i > 0; i--); // Time for flag to set
}
while ((IFG1 & OFIFG) != 0); // OSCFault flag still set?
BCSCTL2 |= SELM_3; // MCLK = LFXT1 (safe)
ME2 |= UTXE0 + URXE0; // Enabled USART0 TXD/RXD
UCTL0 |= CHAR; // 8-bit character
UTCTL0 |= SSEL0; // UCLK = ACLK
UBR00 = 0X41;//0x74; 8MHz/9600 // 3.58Mhz/9600 - 372
UBR10 = 0X03;//0x01; //
UMCTL0 = 0X03;//0x00; // no modulation
UCTL0 &= ~SWRST; // Initalize USART state machine
IE2 |= URXIE0; // Enabled USART0 RX interrupt
_BIS_SR(LPM0_bits + GIE); // Enter LPM0 w/ interrupt
}
#pragma vector=USART0RX_VECTOR
__interrupt void usart0_rx (void)
{
while (!(IFG2 & UTXIFG0)); // USART0 TX buffer ready?
TXBUF0 = RXBUF0; // RXBUF0 to TXBUF0
}
希望能帮到你!
//******************************************************************************
// MSP-FET430P120 Demo - USART0, UART 9600 Echo ISR, HF XTAL ACLK
//
// Description: Echo a received character, RX ISR used. Normal mode is LPM0,
// USART0 RX interrupt triggers TX Echo. Though not required, MCLK = LFXT1.
// Baud rate divider with 3.58Mhz XTAL @9600 = 3.58MHz/9600 = 372 (0174h)
// ACLK = MCLK = UCLK0 = LFXT1 = 3.58MHz
// //* USART0 interrupt flags are in different SFR's from other MSP430's *//
// //* An external 3.58Mhz XTAL on XIN XOUT is required for ACLK *//
//
//
// MSP430F123(2)
// -----------------
// /|\| XIN|-
// | | | 3.58MHz
// --|RST XOUT|-
// | |
// | P3.4|------------>
// | | 9600 - 8N1
// | P3.5|<------------
//
//
// M. Buccini
// Texas Instruments Inc.
// Feb 2005
// Built with CCE Version: 3.2.0 and IAR Embedded Workbench Version: 3.21A
//******************************************************************************
#include <msp430x12x2.h>
void main(void)
{
volatile unsigned int i;
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
P3SEL |= 0x30; // P3.4,5 = USART0 TXD/RXD
BCSCTL1 |= XTS; // ACLK = LFXT1 = HF XTAL
do
{
IFG1 &= ~OFIFG; // Clear OSCFault flag
for (i = 0xFF; i > 0; i--); // Time for flag to set
}
while ((IFG1 & OFIFG) != 0); // OSCFault flag still set?
BCSCTL2 |= SELM_3; // MCLK = LFXT1 (safe)
ME2 |= UTXE0 + URXE0; // Enabled USART0 TXD/RXD
UCTL0 |= CHAR; // 8-bit character
UTCTL0 |= SSEL0; // UCLK = ACLK
UBR00 = 0x74; // 3.58Mhz/9600 - 372
UBR10 = 0x01; //
UMCTL0 = 0x00; // no modulation
UCTL0 &= ~SWRST; // Initalize USART state machine
IE2 |= URXIE0; // Enabled USART0 RX interrupt
_BIS_SR(LPM0_bits + GIE); // Enter LPM0 w/ interrupt
}
#pragma vector=USART0RX_VECTOR
__interrupt void usart0_rx (void)
{
while (!(IFG2 & UTXIFG0)); // USART0 TX buffer ready?
TXBUF0 = RXBUF0; // RXBUF0 to TXBUF0
}