Other Parts Discussed in Thread: MSP430G2553
如何在msp430g2553上用定时器输出两路频率、占空比可调的方波?求源码,如果有已有的例程更好,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430G2553
如何在msp430g2553上用定时器输出两路频率、占空比可调的方波?求源码,如果有已有的例程更好,谢谢!
官网例程里没有两路的。一路pwm输出的好像也没有可调频率、占空比的。不过很简单的,下面例程调节CCR0和CCR1就能调整频率和占空比。一路会了,两路就简单了。
//******************************************************************************
// MSP430G2xx3 Demo - Timer_A, PWM TA1, Up/Down Mode, 32kHz ACLK
//
// Description: This program generates one PWM output on P1.2 using
// Timer_A configured for up/down mode. The value in CCR0, 128, defines the
// PWM period/2 and the value in CCR1 the PWM duty cycle. Using
// 32kHz ACLK as TACLK, the timer period is 7.8ms with a 75% duty cycle on
// P1.2. Normal operating mode is LPM3.
// ACLK = TACLK = LFXT1 = 32768Hz, MCLK = default DCO
// //* External watch crystal installed on XIN XOUT is required for ACLK *//
//
// MSP430G2xx3
// -----------------
// /|\| XIN|-
// | | | 32kHz
// --|RST XOUT|-
// | |
// | P1.2/TA1|--> CCR1 - 75% PWM
//
// D. Dang
// Texas Instruments, Inc
// December 2010
// Built with CCS Version 4.2.0 and IAR Embedded Workbench Version: 5.10
//******************************************************************************
#include <msp430.h>
int main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
P1DIR |= 0x0C; // P1.2 and P1.3 output
P1SEL |= 0x0C; // P1.2 and P1.3 TA1/2 otions
CCR0 = 128; // PWM Period/2
CCTL1 = OUTMOD_6; // CCR1 toggle/set
CCR1 = 32; // CCR1 PWM duty cycle
TACTL = TASSEL_1 + MC_3; // ACLK, up-down mode
__bis_SR_register(LPM3_bits); // Enter LPM3
}